Debuk MKL04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debuk MKL04

754 Views
vincenzogiudici
Contributor I

Hello I am developing with kl04 but when do I debug with usb universal multilink, the device connects but immediately generates an interrupt that invokes "PE_ISR (Cpu_ivINT_Hard_Fault)"

It 'a test firmware where I implement only the CPU model with Processor Expert.

How can I fix?

thanks

Labels (1)
0 Kudos
4 Replies

591 Views
BlackNight
NXP Employee
NXP Employee

Hi Vincenzo,

which KL04 exactly? And are you using Kinetis Design Studio V1.1.1?

I think the problem could be your startup code. Below is my KL04Z32 linker file:

/* Generate a link error if heap and stack don't fit into RAM */

__heap_size = 0x0400;                  /* required amount of heap  */

__stack_size = 0x0100;                 /* required amount of stack */

MEMORY {

  m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x000000C0

  m_text      (RX) : ORIGIN = 0x00000410, LENGTH = 0x00007BF0

  m_data      (RW) : ORIGIN = 0x1FFFFC00, LENGTH = 0x00001000

  m_cfmprotrom  (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010

}

Increase the heap size to see if this helps. I think the problem on your side is that the ANSI library code crashes because the library in KDS uses too much heap space.

Otherwise, I have a Processor Expert component which helps to identify the hard fault, see:

A Processor Expert Component to Help with Hard Faults | MCU on Eclipse

The component is available from SourceForge (see McuOnEclipse Releases on SourceForge | MCU on Eclipse)

I hope this helps,

Erich

591 Views
vincenzogiudici
Contributor I

Thanks for the reply.

Use MKL048VFK4 SQN with Kinetis Design Studio V1.1.1

Until now I have developed with the FRDM-KL05Z and now I have to go on my microcontroller that is the MKL048VFK4 SQN.

Having done the test with Processor Expert thought I did not have these types of problems.

0 Kudos

591 Views
EmilioBrivio
Contributor III

Vincenzo,

I think that there is a  a possible problem in the generation of the processorexpert.ld file for KL04Z8 in KDS 1.1.1 :

the data lenght is 0x00000500 I shoud expect 0x00000400.

  m_data      (RW) : ORIGIN = 0x1FFFFE00, LENGTH = 0x00000500

In the startup.c there is the zero_fill_bss function and exceding the 1K hw limit you had the hardfault.

Change  the processorexpert.ld line and you should solve your issue.

   

Ciao Emilio.

0 Kudos

591 Views
EmilioBrivio
Contributor III

Dear Vincenzo,

If you are using pe pay attention that the ld file is automatically generated by pe if the flag is enabled.

In CPU component inspector check build option and modify there in case you have the flag set.

Regards,

Emilio.

0 Kudos