Using the FRDM-KL25 Board as a USB Keyboard in KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the FRDM-KL25 Board as a USB Keyboard in KDS

Using the FRDM-KL25 Board as a USB Keyboard in KDS

USB Keyboard in KDS

 

Description:

 

A project made in KDS using the FRDM-KL25Z128M4 board as a USB keyboard input.

The LED will flash red while not connected as a USB keyboard, and flash green when it is.

The reset button will press the print screen button.

The reset button can be configured to press any possible key as long as they are correctly #defined.

Use http://www.usb.org/developers/devclass_docs/Hut1_11.pdf as a reference for keys.

Strings may also be output, see the commented out H1DK1_SendStr call in main.c for an example.

 

Sections of code taken from http://mcuoneclipse.com/2013/06/30/using-the-frdm-kl25z-as-usb-keyboard/

ラベル(1)
添付
コメント

Is there any example for media keyboard?

評価なし
バージョン履歴
最終更新日:
‎06-30-2014 07:54 AM
更新者: