将Gui-Guider项目导出,移植到开发板

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

将Gui-Guider项目导出,移植到开发板

Jump to solution
1,307 Views
bobbyzhang
Contributor I

hi,我想要在我的服务器上交叉编译我在Gui-Guider配置好的项目,我将custom、generated下面的代码都复制到我的服务器上然后配置好环境,但是在generated目录下widgets_init.c最后有一个lv_video_play接口,这个接口编译报错,提示undefined reference to `lv_video_play',请问Gui-Guider1.6.1以及更高版本用的lvgl的版本是哪个?

0 Kudos
Reply
1 Solution
1,252 Views
Alex_Wang
NXP Employee
NXP Employee

Hi, @bobbyzhang 

        您好,目前视频控件只在NXP提供的LVGL库中可以正常使用。LVGL库中并没有lv_vedio_play()。

Best regards, Alex

View solution in original post

0 Kudos
Reply
3 Replies
1,276 Views
Alex_Wang
NXP Employee
NXP Employee

Hi, @bobbyzhang 

        GUI guider 1.6.1 lvgl 版本有两个可以选择,分别是v7.10.1和v8.3.5,我们最近也发布了最新版本的GUI guider 1.7.0版本,其lvgl版本位v7.10.1和v8.3.10。

Best regards, Alex

0 Kudos
Reply
1,271 Views
bobbyzhang
Contributor I

hi, @Alex_Wang  我使用的是Gui-Guider 1.6.1的版本,我在我的服务器上也配置了lvgl v8.3.5的版本,但是当我将我用Gui-Guider搭建好的项目中的custom和generated移植并交叉编译的时候报错。具体报错内容可以看我的附件截图。说真的,我并没有在lvgl里面查询到报错的那个接口。

0 Kudos
Reply
1,253 Views
Alex_Wang
NXP Employee
NXP Employee

Hi, @bobbyzhang 

        您好,目前视频控件只在NXP提供的LVGL库中可以正常使用。LVGL库中并没有lv_vedio_play()。

Best regards, Alex

0 Kudos
Reply