why freemaster can't load communication library?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

why freemaster can't load communication library?

跳至解决方案
1,084 次查看
tiasum
Contributor I

i can use jlink to connect my MCU,but in freemaster it seems that can't load the jlinkarm.dll file.anyone know how to fix it?need help,thank you.1.png2.png3.png

标记 (1)
0 项奖励
1 解答
1,064 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello,

I confirm the JLinkARM.DLL from version 6.00i cannot be loaded due to some missing API which FreeMASTER depends on.

Is it possible for you to update to the latest JLink version 7.86?

The oldest JLink we were testing with the FreeMASTER 2.5 and 3.x back in 2018 was version 6.32h, so this one should work as well. But in general, it is a good idea to keep the JLink software up-to-date.

Regards,
Michal

 

 

在原帖中查看解决方案

0 项奖励
5 回复数
1,080 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello,

FreeMASTER requires to locate some specific functions in the JLinkARM.dll. When it does not find them, the loading fails. Maybe your version of the DLL is older (or much newer?) than the FreeMASTER expects and the set of functions differs.

Can you tell what JLink package version you are using? We can download the same from Segger and retest the FreeMASTER compatibility.

Thanks,
Michal

 

0 项奖励
1,074 次查看
tiasum
Contributor I

my jlink version is v6.00i and freemaster version is 3.2

0 项奖励
1,065 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello,

I confirm the JLinkARM.DLL from version 6.00i cannot be loaded due to some missing API which FreeMASTER depends on.

Is it possible for you to update to the latest JLink version 7.86?

The oldest JLink we were testing with the FreeMASTER 2.5 and 3.x back in 2018 was version 6.32h, so this one should work as well. But in general, it is a good idea to keep the JLink software up-to-date.

Regards,
Michal

 

 

0 项奖励
1,061 次查看
tiasum
Contributor I

ok,i will try it.thx u!

0 项奖励
1,009 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello,

is anything new in this case?

Thanks,
Michal

 

0 项奖励