5744P, When CAN0 is being used , is it possible to still use CAN0 to connect with FreeMaster ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

5744P, When CAN0 is being used , is it possible to still use CAN0 to connect with FreeMaster ?

952 Views
ChenBowen
Contributor II

Dear Expert: 

      MPC5744P,  CAN0 is being used .  Is it possible to use CAN0 to do calibration at the same time?

or I need to use CAN1 instead?  By the way , I plan to use the FreeMaster SDK in S32DS.

0 Kudos
Reply
2 Replies

943 Views
ChenBowen
Contributor II

Expert,please answer my question

0 Kudos
Reply

934 Views
iulian_stan
NXP Employee
NXP Employee

Hi @ChenBowen,

Unfortunately, CAN interface can not be used simultaneously by FreeMASTER and other application.

The reason is that FreeMASTER Driver will read all message coming via the assigned CAN interface keeping those that are addressed to it (by checking the CAN frame ID) and discarding any other messages.

0 Kudos
Reply