5744P, When CAN0 is being used , is it possible to still use CAN0 to connect with FreeMaster ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

5744P, When CAN0 is being used , is it possible to still use CAN0 to connect with FreeMaster ?

1,086 次查看
ChenBowen
Contributor II

Dear Expert: 

      MPC5744P,  CAN0 is being used .  Is it possible to use CAN0 to do calibration at the same time?

or I need to use CAN1 instead?  By the way , I plan to use the FreeMaster SDK in S32DS.

0 项奖励
回复
2 回复数

1,077 次查看
ChenBowen
Contributor II

Expert,please answer my question

0 项奖励
回复

1,068 次查看
iulian_stan
NXP Employee
NXP Employee

Hi @ChenBowen,

Unfortunately, CAN interface can not be used simultaneously by FreeMASTER and other application.

The reason is that FreeMASTER Driver will read all message coming via the assigned CAN interface keeping those that are addressed to it (by checking the CAN frame ID) and discarding any other messages.

0 项奖励
回复