TDM/I2S communication to TFA9896

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TDM/I2S communication to TFA9896

771 次查看
morten
Contributor I

I am using the TFA9896 to collect audio signals over the I2S line, but the collected data sounds really lousy.

The transmitting device has a Clock on 256kHz, and a Frame Sync on 8kHz.

The TFA9896 collects data with a Clock on 1.536MHz, and a Frame Sync on 48kHz.

I am collecting signals on the TFA's "I2S IN1" line with their corresponding BCK, WS and DATA pins.

I should be able to change the Sync frequency on the TFA9896 with I2C, by sending 0x00 & 0x90 to address 0x04, but when I change the configurations as the datasheet says, it doesn't seem to change the actual Sync frequency at all when I measure the signals. 

Am I using the correct I2S inputs pins, or are there pins designed for the TDM configurations?

Am I using the correct configurations to change the frequencies?

0 项奖励
回复
0 回复数