Hello,
I have problem with DMA SCI on receiver idle interrupt.
I wrote the codes of SCI receiver by DMA and it works well.
But when I try to add receiver idle interrupt, I can not find where the receiver idle interrupt vecteor is.
I have to search the whole <MC56F847xx Reference Manual> but no more information except bellows:
At the middle-left of the Figure 35-28, there is a receiver idle interrupt Request.
But it does not exist in Table 3-10. Interrupt Vector Table:
And I can not find any relative information in CodeWarrior PE.
Please help me, thanks.
Hi, WangJun,
I suppose that the Receiver idle can trigger interrupt vector 52. You can enable the Receiver idle interrupt by setting the RIIE bit QSCIx_CTRL2, in the ISR of vector 52, you can check the RIDLE bit in QSCIx_STAT, if it is set you can see that Receiver idle happens.
As a test, in the ISR of vector 52, you can check the RIDLE bit, if it is set, toggle a GPIO. You can check the GPIO pin waveform to know if the receiver idle happens or not.
BR
XiangJun Rong
Hi, Jun,
Pls refer to the vector table, there are 2 interrupt vectors for the SCI0 receiver, so I suspect the idle interrupt of receiver is included in vector 51 or 52, especially 52.
You can have a try by generating the receiver interrupt and set a break point in two ISR and check which is entered.
BR
XiangJun Rong
Hi, WangJun,
I got feedback from design team, the SCI0 Receiver idle interrupt is not routed to interrupt table vector by mistake, so SCI0 receiver idle interrupt can not be triggered. We will document the issue in the errata.
Thank you for pointing the error.
BR
Xiangjun Rong
Hi, Mr.rong
I tested many times accordding to your suggestion.
I enabled the RFIE & RIIE, and the DMA transported whole message correctly as below:
when a message ended, I checked the relative registors as bellow: RIDLE Flag is set.
but no any interrupt requist pending up: