MC56F8006的ADC模块寄存器怎样用

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC56F8006的ADC模块寄存器怎样用

1,071 次查看
liuzhen
Contributor I

有人能给下MC56F8006的相关例程吗?尤其是关于ADC模块寄存器的

标签 (1)
0 项奖励
3 回复数

795 次查看
TICS_Fiona
NXP Employee
NXP Employee

You can get an example project for the peripherals by creating a new project in Classic CodeWarrior v8.3 from "Processor Expert Example Stationery", then select "DemoApplications -> HWBeans -> 56F800x->… (e.g ADC).

CodeWarrior v8.3 can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励

795 次查看
liuzhen
Contributor I

MC56F80xx系列的完整的例程您有吗,

0 项奖励

795 次查看
khalil001
Contributor II

你好,在吗?可以加下你QQ或者微信交流一下吗?我也在用这个

0 项奖励