I have a MC56F8257DSC please help me how to create new project & simple demo program to toggle GPIO bits of any port, should i use new project wizard or processor expert??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I have a MC56F8257DSC please help me how to create new project & simple demo program to toggle GPIO bits of any port, should i use new project wizard or processor expert??

2,203 次查看
akshaykatkar
Contributor I

I have a MC56F8257DSC please help me how to create new project & simple demo program to toggle GPIO bits of any port, should i use new project wizard or processor expert??

标签 (1)
0 项奖励
7 回复数

2,005 次查看
ankur_kala
NXP Employee
NXP Employee

Hi Akshay,

You can use Processor Expert to make a quick sample application. Use BitIO under Component Library--> CPU Internal Peripherals --> Port I/O. You can also use PE function Bit1_NegVal(); to negate the current value of port pin which effectively would keep it toggling.

0 项奖励

2,005 次查看
akshaykatkar
Contributor I

thank you. but a new problem i am facing is with debugger 56800e gdi protocol: an error occurred while trying to write memory and the debugger cannot write memory please help me to fix this problem please reply as soon as possible

0 项奖励

2,005 次查看
ankur_kala
NXP Employee
NXP Employee

Hi Akshay,

what is the hardware setup you are using. CW version,  Debugger, Board??

0 项奖励

2,005 次查看
akshaykatkar
Contributor I

did you get the solution

On Fri, Apr 25, 2014 at 11:23 AM, Akshaya Katkar

0 项奖励

2,005 次查看
ankur_kala
NXP Employee
NXP Employee

Hi Akshay,

I am trying to get hold of a 8257 TWR card. As soon as I have one, I will try and check.

0 项奖励

2,005 次查看
akshaykatkar
Contributor I

this is the error message i am getting

On Thu, Apr 24, 2014 at 4:20 PM, Akshaya Katkar

0 项奖励

2,005 次查看
akshaykatkar
Contributor I

the image of board is attached it is TWR-MC56F8257...And works with OSBDM

connection.... Debugger board

On Wed, Apr 23, 2014 at 4:40 PM, Ankur Kala

0 项奖励