ADC16 problem of MC56F84789

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC16 problem of MC56F84789

1,114件の閲覧回数
jero17
Contributor I

1. GPIOA11/ANC19 is the only input pin of ADC16

2.Input trans-conduct Amp shares the same VDDA of the DSC, 3.3Vdc

3. conversion time 4uS, Sample time 20=long

4.Init code:

setReg32(ADC16_SC1A, 0x1FUL);
setReg32(ADC16_SC2, 0x44UL);
setReg32(ADC16_SC3, 0x0eUL);
setReg32(ADC16_CFG1, 0x5cUL);
setReg32(ADC16_CFG2, 0x04UL);

5. Synchronous Triggered, DMA read

 

Problem:

1.After 2-10 days normal running, ADC16 result becomes noisy and unpredictable. And some fixed value like 0x07f7 or 0x1ff7 may come out frequently.(input amp and signal source are checked OK)

2. Meanwhile, other analog parts of the DSC such as ADC12 and DAC12 or Comparators work well.

3. Till now, there are at least 5 DSCs suffered from the same problem one by one.

 

Help please!

ラベル(1)
0 件の賞賛
4 返答(返信)

724件の閲覧回数
ruvimelaver
Contributor II

Hello ,

Please advise date code of the part .

Thanks

Ruvi

0 件の賞賛

724件の閲覧回数
jero17
Contributor I

Hi,

I am looking forward to your suggestion.

Thanks

Wang Jun

1031915144.jpg

0 件の賞賛

724件の閲覧回数
mohammad_kamil
NXP Employee
NXP Employee

DTE: 1435 indicates it  year 2014, 35th Week of manufacturing

0 件の賞賛

724件の閲覧回数
jero17
Contributor I

the 6th, last friday

0 件の賞賛