Running oprofile on mcf5445x platforms

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running oprofile on mcf5445x platforms

980件の閲覧回数
mjlear
Contributor I

Hello all - I have an mcf54455 evb and I'm trying to run oprofile. I'm running 2.6.23 and 2.6.25 kernels (the former from ltib-mcf5445x-20071214, the latter obtained from the gpp). However, both kernels are missing the config options to enable profiling. It seems, to all intents and purposes, that profiling just isn't supported in the coldfire kernels. Is this correct?

 

Has anybody actually got oprofile running and working successfully on coldfire? I have had a dig around the forum and found various postings but nothing I can glean any information from.

 

Any feedback would be much appreciated.

Thanks.

ラベル(1)
0 件の賞賛
2 返答(返信)

334件の閲覧回数
fsl_linux_spt
Contributor III

Oprofile is not supported.  I looked around on the internet and it does not look like this is supported on any coldfire processor.

 

Looking in the kernel source this option is dependent on HAVE_OPROFILE.  There are several arch/<specific_arch>/Kconfig files that "select HAVE_OPROFILE" but the m68k and m68knommu do not.

0 件の賞賛

334件の閲覧回数
mjlear
Contributor I
Apart from readprofile & /proc/profile (standard kernel profiling infrastructure), what profiling environment is supported on coldfire (if any)?
0 件の賞賛