MCF54418CMJ250 2 RMII MODE DESIGN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF54418CMJ250 2 RMII MODE DESIGN

345 Views
luna_liang
Contributor II

基于MCF54418CMJ250这款芯片,如果百兆网使用RMII模式,应该如何设计。谢谢。

目前,我们使用的50MHz的时钟是外部晶振,然后通过一个时钟buffer,输出两路50MHz时钟,分别供给MCF54418(MAC)和两颗TI的DP83848(PHY)。当前设计50MHz时钟到MAC和到PHY的走线距离未做等长处理。

下面是MCF54418和外部时钟的具体线路图,我们使用了两路RMII网口。

luna_liang_0-1711095232754.png

 

 

luna_liang_1-1711095232771.png

 

0 Kudos
1 Reply

319 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Luna,

Unfortunately, there is no dedicated document for ColdFire Ethernet RMII layout guideline. I would recommend customer to refer AN13335 PCB design guideline for Auto Ethernet , especially chapter 2.1.2 Routing and trace distance.

Wish it helps.

Mike

0 Kudos