End of Life Parts (M5225x, M5221x)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

End of Life Parts (M5225x, M5221x)

729 Views
mjbcswitzerland
Specialist V

Hi All / Freescale

 

Please could the following be clarified?

 

The following end of life announcement - http://www.freescale.com/files/shared/doc/pcn/PCN15389.htm

is showing some parts that are being used in production as being discontinued due to low sales, but replacement types are not obvious.

 

In particular M5225x parts that are being used in 144 MAPBGA are to be discontinued, meaning that there is no MAPBGA parts more offered - apart from the MCF52256VN80 which has 256k Flash, 32k SRAM and commerical temperature range. This will affect a new product that is presently ramping up, which requires the MAPBGA in extended temperature range (although the memory size may still just fit). Would it not make more sense to keep the MCF52259CVN80 rather than the MCF52256VN80 since that should cover all production in MAPBGA?

 

In the case of M5221x parts mainly LQFP and QFN devices are being discontinued. The remaining ones in this package are however smaller and slower than the ones that are presently being used for production, and have less UARTs.

 

In both cases a redesign of the boards to use different packages (only last purchase has expired) look unavoidable.

 

There are some other Coldfires on the list but I didn't check those closely but they may affect other manufacturers.

 

Finally, the discontinuation is not shown for many parts on the product selection web page, where they are shown as active (some with J at the end are shown as discontinued but their recommended replacement parts then point to parts on the list which will also be discontinued).

 

Regards

 

Mark

 

P.S. The images below show quickly the changes with regards to the two families mentioned above.

4601_4601.PNGM5225X.PNG4602_4602.pngM5221x.png

Labels (1)
Tags (3)
0 Kudos
2 Replies

360 Views
mjbcswitzerland
Specialist V

Hi All

I the meantime one of the distrubutors who passed on the PCN has informed that it was a mistake and retracted, whereby only the parts with J on the end are in fact affected.

"Hoping" that this is correct for the moment... can anyone confirm??

Regards

Mark

0 Kudos

360 Views
eric_limbert
NXP Employee
NXP Employee

Hi Mark,

Freescale issued an update to PCN15389 to correct the list of affected part numbers.  The update is PCN15389A:

http://cache.freescale.com/files/shared/doc/pcn/PCN15389A.htm

Freescale also issued PCN15414 to explicitly remove some part numbers from the original PCN (15389).  PCN15414 can be found at:

http://www.freescale.com/files/shared/doc/pcn/PCN15414.htm

To find the status of a specific part number, please visit freescale.com and perform and "Orderable Part" search for that part number.  The status is displayed in the results.  If you want to know about PCNs that affect that part, click the "information" icon to the right of the part number in the search results.  The icon looks like a document containing a lower-case letter "i".  In the window that appears, scroll down to the "Product/Process Change Notice (PCN)".  There, all PCNs are listed with clickable links to view generic copies of the notices.

For part number MC56F8006VWL, here is how the PCN information can be retrieved:
PCNs on freescale.com 14JUN13.png

Hope this helps.

0 Kudos