Cold fire 52235 and 802.15.4 MAC application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cold fire 52235 and 802.15.4 MAC application

2,283 次查看
kj
Contributor I
Hello forum members,

Does any one knows where can I get 802.15.4 MAC libraries for m2235 and mywireless App example.

I am working with MFC52235EVB but on net I can only get MAC for 5282 802.15.4_CF5282_MAC.zip.

Can I use these MAC libs on with uCLinux on 52235?

----
Santosh
标签 (1)
0 项奖励
6 回复数

585 次查看
kj
Contributor I
I managed to run 8021.5.4 MAC on MCF52235.
0 项奖励

585 次查看
RickN
Contributor I
Hi,
 
  I would try the MAC provided for the 5213 as it is very similar to the 5223x MCUs.
 
  Thanks,
 
     Rick
 
 
0 项奖励

585 次查看
kecart
Contributor III
Rick,  Isn't that code the old stuff that was acquired by TI and no longer supported?  Does anyone know when there will be a supported 802.15.4/ZigBee stack for the ColdFire?  2 years ago at FTF it was supposedly next on the list but has been push out multiple times.
0 项奖励

585 次查看
RickN
Contributor I
Hi KJ,
 
   The MCF52235 doesn't have enough resources to run uCLinux, so you need to consider other options.
 
   I checked the Freescale website and only found the 5282 MAC, as you mentioned.   I would recommend using the SMAC, if possible, because you get the source code, which puts you in a strong position for debugging and enhancing the driver.   You might also try using the MC1320x 802.15.4 transceivers for your project. 
 
 
   Thanks,
 
    Rick
0 项奖励

585 次查看
WOLF
Contributor I
I have been trying to get the MC1320x Rf daughter card to work on the M52233Demo boards.  but the code i received from freescale wont work. All controll lines were confgured incorrecty (I figure for a different board) I have been able to get past most of that. and I can read and write to the MC13202 via SPI, but cant get past that.    does anyone have a project that works?
0 项奖励

585 次查看
kj
Contributor I
Hello RicKN,
Thanks,Let say I dont want to use uCLinux.
I can live with code warrior for coldfire but it must run 802.15.4 stack.
I am working on a project where I already have 802.15.4 based coordinator running on HCS08 GT60 and MC13192.
I was in process to replace GT60 with MCF5335 and I want to run the 802.15.4 stack on top of it and I have very less time to do that, its less than 2 working days.
Freescale websites mentions that 802.15.4 MAC libraries are availble for all coldfire processor. On internet then why its only for 5283 5213.

I can try SMAC but finally i need 802.15.4 stack over it, even I manage to run SMAC I will be in same position. I seek some break through solution.
0 项奖励