Hello !
It's not my first time here but I ask to my teachers and they can't help me because they never work with DSP at all. Freescale community and other forum are my only way to find help. So if I'm here it is because I'm stuck again ...
This time I tried to make a simple lowpass filter inspired by the technic from the Benchmark programme of the 56k user manuel.
The equation to implement is : Y(n) = 0.061*x(n) + 0.061*x(n-1) + 0.877*y(n)
Here is the code :
...
move #000208,r4
move #2,m4
move #TableCoeff,r0
do #3,_enddo ;Load TableCoeff to y memory
move y:(r0)+,a
nop
move a,y:(r4)+
_enddo ;end loadTableCoeff
move #000200,r0
move #2,m0
clr a
AudioLoop
jclr #RightRx,x:LRFlag,*
bclr #RightRx,x:LRFlag
move x:RxBuffBase,a ; <- Input ADC left
nop
move a,x:(r0)
rnd a x:(r0)+,x0 y:(r4)+,y0
mpy y0,x0,a x:(r0)+,x1 y:(r4)+,y0 ; a = 0.061*x(n)
mac y0,x1,a x:(r0)+,x0 y:(r4)+,y0 ; a = a + 0.061*x(n-1)
macr y0,y1,a ; a = a + 0.877*y(n-1)
move x:(r0)+,x0 ; take out x(n)
move x0,x:(r0)+ ; x(n) -> x(n-1)
move a,x:(r0)+ ; y(n) -> y(n-1)
move a,x:TxBuffBase ; a = y(n) -> DAC left output
jmp AudioLoop
...
The memory mapping is :
X memory :
000200 : X(n)
000201 : X(n-1)
000202 : Y(n-1)
Y memory :
000208 : coefficient b0 (0.061)
000209 : coefficient b1 (0.061)
000210 : coefficient a1 (0.877)
When I test the code, I have an output signal but its amplitude not change with an increase of frequency. So what's wrong ?
已解决! 转到解答。
Hi Maxime,
I have not analyzed your code yet, but at first glance it looks well structured. I have a few questions though.
What is the cutoff frequency supposed to be? What frequencies are you feeding it?
The amplitude should not change at all until you approach the cutoff frequency, at which point it should be attenuated about 3db. Could it be that you haven't reached the cutoff frequency yet? I can't tell what the cutoff should be, as I don't know the sample rate.
The cutoff frequency is about 1kHz and the sample frequency is 48kHz.
I tested the filter with an oscilscope :
At F.input < 1khHz
Input = 900mV
Output = +-160mV
I also tested the loading of coefficients table to Y memory and it work well.
But I remember that the Benchmark program of the 56k manuel divide all coefficients by 2. I did not divide it. Should I do it ?
This program is primarily used to teach me how to properly use the assembler technics. It treats the audio bandwidth