in codewarrior 6.3 i cannot choose CF_M537x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

in codewarrior 6.3 i cannot choose CF_M537x

2,532件の閲覧回数
VeronicaFNX
Contributor I
Hello,
 
i bought an mcf5373L evaluation board. I want to create a project of type "Coldfire Stationery" but I cannot choose CF_M537x because it not exists. I looked for an patcher but i find nothing.  I need another codewarrior version? what can i do?
 
codewarrior 6.3 and mcf5373L
 
Thanks. :smileywink:
ラベル(1)
タグ(1)
0 件の賞賛
返信
9 返答(返信)

492件の閲覧回数
J2MEJediMaster
Specialist I
0 件の賞賛
返信

492件の閲覧回数
VeronicaFNX
Contributor I
I cannot to install it because i have got an error that it says,
 
"A qualified installation of codewarrior Developer Studio could not be found in the forder specifier. Please check the forder selected and try again".
 
i choose the forder C:\Archivos de programa\freescale\codewarrior for coldfire v6.3\
 
i don't know that occurs.
 
0 件の賞賛
返信

492件の閲覧回数
J2MEJediMaster
Specialist I
For some reason your system layout appears to be confusing the installer. I would just try the default settings to begin with, and then try the path C:\Archivos de programa\freescale\ to see if the installer can locate the CodeWarrior directory on its own.

---Tom

0 件の賞賛
返信

492件の閲覧回数
VeronicaFNX
Contributor I
No, thus it does not work either. Not that I can do.
0 件の賞賛
返信

492件の閲覧回数
J2MEJediMaster
Specialist I
Two last things I can think of to try:

First try changing C:\Archivos de programa\freescale\ to C:\Program Files\freescale\, and run the installer. If that works, the problem was that the installer didn't recognize the different name for the Program Files directory. Be sure to change the directory name back.

Second, if that doesn't work, something must be botched in the CodeWarrior install. So, uninstall CodeWarrior using the Windows Add or Remove Programs control panel. Then, reinstall CodeWarrior. If you can, try to use the defaults, especially on the directory paths. Then try running the 6.3.1 installer.

If that doesn't work, you'll have to file a service request.

---Tom

0 件の賞賛
返信

492件の閲覧回数
VeronicaFNX
Contributor I
Not. I think that is a licence problem, i don`t know.
 
Anyway, thanks.
0 件の賞賛
返信

492件の閲覧回数
VeronicaFNX
Contributor I
the solution is to replace "freescale" by "metrowerks",
 
c:\Archivos de programa\metrowerks\codewarrior......
 
i can to install the patch, but the patch 6.3.1 is not the solution because still the micro is not on my list. I don't know the codewarrior version that i need.
0 件の賞賛
返信

492件の閲覧回数
J2MEJediMaster
Specialist I
You need to Submit a Service Request with Freescale to have this looked into. Sorry I couldn't be of more help, but this has progressed beyond my trouble-shooting skills...

---Tom

0 件の賞賛
返信

492件の閲覧回数
VeronicaFNX
Contributor I
thanks, I will do it
0 件の賞賛
返信