Hi,
I want to use following command on CCS prompt:
ccs::read_mem ::chain_pos ? address_hi? address size space count
My queries are :
1. What is chain_pos?
2. What is address_hi?
Please help me.
Thanks & Regards,
Kavita
解決済! 解決策の投稿を見る。
Use the Debugger Shell to access memory. It is easier to use and supported.
Hi Heinz, how do you run the debugger shell ? is this part of CCS ?
This is the CCS I am running if the debugger shell is in another version :
% show version
CCS Linux Release Build 365p0
CodeWarrior Connection Server version {4.13}
(C) Copyright 2003-2010 Freescale Semiconductor, Inc. ALL RIGHTS RESERVED
Thanks
Sinan Akman
Hi,
You can open the debugger shell from CW: Window -> Show View -> Debugger Shell.
Marius
Hi, Kavita
Yes, as Heinz said. You can use "mem" or "display" in debugger shell, type "help mem" or "help display" for detail description of command.