Total ROM size and RAM size - CW for MPC55xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Total ROM size and RAM size - CW for MPC55xx

2,548 Views
james-lee
NXP Employee
NXP Employee
Hello,
 
I am using CodeWarrior for MPC55xx v2.3 and would like to know the total ROM size and RAM size of my application program. When I use CW for S12X, I could find them in the .map file as follows.
 
Summary of section sizes per section type:
READ_ONLY (R):        2C70 (dec:    11376)
READ_WRITE (R/W):      34C (dec:      844)
NO_INIT (N/I):          CD (dec:      205)
 
But, I could not find any information in the .map file for MPC55xx. Is there any option to add these information? Please give your advice.
 
Best regards,
James
 
 
Labels (1)
0 Kudos
Reply
1 Reply

1,156 Views
stanish
NXP Employee
NXP Employee
Hello J.W.

Following thread might help you to answer your question:

http://" rel="nofollow" target="_blankhttp://forums.freescale.com/freescale/board/message?board.id=CWCFCOMM&message.id=2262&query.id=1675#...

Stanish


Message Edited by stanish on 2008-12-01 01:03 PM
0 Kudos
Reply