TBLCF BDM can't open memory configuration file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TBLCF BDM can't open memory configuration file

Jump to solution
2,282 Views
bluehacker
Contributor III

Hi, eveyone!

 I am now developing one mcf52211 board. and buy one TBLCF BDM pod. and using cw 7.1 special edtion. But when I click"debug" button, I always get:"could not open memory configuration file"; I don't know how to set the memoery configuration file in CW. any suggestions?

thanks in advance! 

Labels (1)
0 Kudos
1 Solution
521 Views
J2MEJediMaster
Specialist I

First, did you use the CodeWarrior Project wizard to set up your project, or start it from scratch (Empty Project)? If you use the wizard, it normally sets up the configuration file for you. You can select the memory configuration file to use from the project settings panel. Type Alt+F7 to bring up the project's settings panel. Select the CF Debugger Settings panel. On this panel you'll see the option for Use Memory Configuration File. You can use the Browse button to choose a different memory configuration file, one that better matches your target board.

 

---Tom

View solution in original post

0 Kudos
2 Replies
522 Views
J2MEJediMaster
Specialist I

First, did you use the CodeWarrior Project wizard to set up your project, or start it from scratch (Empty Project)? If you use the wizard, it normally sets up the configuration file for you. You can select the memory configuration file to use from the project settings panel. Type Alt+F7 to bring up the project's settings panel. Select the CF Debugger Settings panel. On this panel you'll see the option for Use Memory Configuration File. You can use the Browse button to choose a different memory configuration file, one that better matches your target board.

 

---Tom

0 Kudos
521 Views
bluehacker
Contributor III
Hi, I am now solved the problem,. the reason is I use chinese name for my project folder. cw seem not know chinese correctly. thanks!
0 Kudos