QCVS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QCVS

4,549件の閲覧回数
hv
Contributor II

If I download an eval CodeWarrior, does QCVS come with that?  Thanks!

ラベル(1)
0 件の賞賛
6 返答(返信)

3,985件の閲覧回数
addiyi
NXP Employee
NXP Employee

You can use also the update site. Go to Help > Install New Software and select FSL PA QCVS - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win from drop down menu. 

Adrian

0 件の賞賛

3,985件の閲覧回数
hv
Contributor II

Thanks!

0 件の賞賛

3,985件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello H VO,

QCVS tool is not included in CodeWarrior for PA, please download QCVS for PA from CodeWarriorNetworked Applications : QCVS|NXP, then open CodeWarrior IDE and install QCVS 4.5 from Help->Install New Software->Add->Archive, specify the installation file path to follow wizards to install QCVS step by step.

Thanks,

Yiping

0 件の賞賛

3,257件の閲覧回数
Chinzw
Contributor I

@yipingwang   Can you share  the  CodeWarrior IDE and install QCVS 4.5 software  in baidu netdisk again ? Thanks a lot 

0 件の賞賛

3,259件の閲覧回数
Chinzw
Contributor I

http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win 

@yipingwang

Can you share QCVS 4.5 in Baidu netdisk again ? Thanks a lot .

0 件の賞賛

3,985件の閲覧回数
hv
Contributor II

Thank you!

0 件の賞賛