The reason of the problem is that I missed patch 'Upgrade 2 for OSEKturbo OS/MPC55xx v.2.2.1 RP, Build 2.2.1.82'
The demo project is working well in MPC5554 EVB.
Now, I'm trying to port 'OSEKturbo OS/MPC55xx v.2.2.1 RP, Build 2.2.1.82' for MPC5567 Unfortunately, the demo project does not worked in MPC5567 EVB rev.A directly.
Do you have demo project of OSEKturbo for MPC5567 ??
When you do the build, does the Errors & Warnings window display that the OSEK Sysgen Generator has run, and did it do so without any warnings or errors? From my own experience (HCS12X platform, though), if the Sysgen Generator doesn't run properly, you get all sorts of odd errors.
---Tom
Message Edited by J2MEJediMaster on 2009-01-0710:13 AM