LS1046 ardb flash program error on JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046 ardb flash program error on JTAG

Jump to solution
1,130 Views
sreeragag
Contributor II

Hi
We are trying to flash Hard coded RCW in LS1046ardb using JATG.
When we do flash operations on QSPI unprotect, blank check work, but cannot erase or program a file.
Also user reference of ls1046ardb says when we use Hard coded RCW, DDR controller and Core should not enabled. How can we program or set-up core and DDR controller disable?
Switch setting used
SW3[1:8]             SW4[1:8]          SW5[1:8]
0b01000110    0b10110011    0b01001111

Also we have tried with switch setting same SW3, SW4. and SW5 0b010011110

Tags (3)
0 Kudos
Reply
1 Solution
785 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Sreerag A G,

Please refer to the first section in this document Use CodeWarrior for ARMv8 to Debug U-boot and Linux Kernel and Bring up Bare Boards to do flash programming. In the default CodeWarrior initialization file OCRAM is used in flash programming rather than DDR.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
786 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Sreerag A G,

Please refer to the first section in this document Use CodeWarrior for ARMv8 to Debug U-boot and Linux Kernel and Bring up Bare Boards to do flash programming. In the default CodeWarrior initialization file OCRAM is used in flash programming rather than DDR.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply