Flash Programmer: Can Not Initialize the target "8270"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Programmer: Can Not Initialize the target "8270"

2,309件の閲覧回数
Kersh
Contributor I
Pleae make sure ".....>myconfig.cfg" exists and it is a valid configuration file. (Which it is).

Additional error information: Interface function IMWProtocol::GetPreferences is unimplmented.


Any Help??
ラベル(1)
タグ(1)
0 件の賞賛
1 返信

637件の閲覧回数
Teo
NXP Employee
NXP Employee
".....>myconfig.cfg" is the board/target initialization file. In case you have a supported board, there's already such init file in CodeWarrior layout.

Assuming you have a Freescale Reference PQ2-FADS board with 8270, then the init file is {CW}\PowerPC_EABI_Support\Initialization_Files\PQ2\PQ27e_init.cfg

Also, note that for convenience, there're all flash programmer specific settings for reference boards stored in CodeWarior layout. After you open flash programmer window, use "Load Settings" button, and browse for {CW}\PowerPC_EABI_Support\Initialization_Files\PQ2\PQ27e_init.cfg
(Assuming you have PQ2-FADS reference board). Make sure you have correct connection settings in flash programmer window after loading new settings.

Regards,
Teo
0 件の賞賛