Editing Reserved Field of RCW using QorIQ Tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Editing Reserved Field of RCW using QorIQ Tool

679 次查看
sl1
Contributor I

Hi, I'm modifying the RCW of the LS1020A device but I'm having an issue with a reserved field.  According to the datasheet of the LS1020A, bits 212-215 are Reserved but the values must be set to 0b1010.  However, I'm unable to change this using the QorIQ Configuration in Code Warrior.  And when I generate the binary file, the values of those reserved fields are 0b0000.  So how can I change this so that it meets the requirement of the datasheet?

 

Thanks.

标签 (1)
0 项奖励
4 回复数

476 次查看
addiyi
NXP Employee
NXP Employee

Please let me know the QCVS version you used and the Rev for LS1020.

Adrian

0 项奖励

476 次查看
sl1
Contributor I

Hi Adrian,

I am using CodeWarrior Development Studio for QorIQ LS series - ARM V7 ISA v10.0.8 with QorIQ Configuration and Validation Suite v4.4.1.  As for the silicon revision, I tried both v1.0 and v2.0 and I see the same thing.  I am in contact with someone who sees bit 212-215 on their configuration screen but they're using CodeWarrior v10.0.4.  I do not know which version of QorIQ Configuration and Validation Suite though.

Thanks.

0 项奖励

476 次查看
addiyi
NXP Employee
NXP Employee

Please update to QCVS 4.5.

Adrian

0 项奖励

476 次查看
sl1
Contributor I

I did that and it now works.

Thanks.

0 项奖励