Hi, I'm modifying the RCW of the LS1020A device but I'm having an issue with a reserved field. According to the datasheet of the LS1020A, bits 212-215 are Reserved but the values must be set to 0b1010. However, I'm unable to change this using the QorIQ Configuration in Code Warrior. And when I generate the binary file, the values of those reserved fields are 0b0000. So how can I change this so that it meets the requirement of the datasheet?
Thanks.
Please let me know the QCVS version you used and the Rev for LS1020.
Adrian
Hi Adrian,
I am using CodeWarrior Development Studio for QorIQ LS series - ARM V7 ISA v10.0.8 with QorIQ Configuration and Validation Suite v4.4.1. As for the silicon revision, I tried both v1.0 and v2.0 and I see the same thing. I am in contact with someone who sees bit 212-215 on their configuration screen but they're using CodeWarrior v10.0.4. I do not know which version of QorIQ Configuration and Validation Suite though.
Thanks.
Please update to QCVS 4.5.
Adrian
I did that and it now works.
Thanks.