Hello,
I'm trying to validate a custom board with a T2080 device.
From codewarrior I can connect to the board and I can access all registers of T2080 processor (LAW, IFC, DDR, ...)
But when I start QCVS in order to use DDR validation toos I get a error "can't connect to server!"
And when I open Validation tab no Target connection is available
I've a valid license for this product.
The CCS server is working properly and detect CWTAP
Can tou help me?
thanks in advance.
Hello,
When I select localhost, automatically changes to remote.
I can’t generate a new target connection, the button is disabled.
De: addiyi
Enviado el: miércoles, 10 de mayo de 2017 12:53
Para: Hernández Sánchez, Sergio
Asunto: Re: - Re: DDR validation tools can't connect to server
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: DDR validation tools can't connect to server
reply from Adrian Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in CodeWarrior for QorIQ - View the full discussion<https://community.nxp.com/message/904078?commentID=904078&et=watches.email.thread#comment-904078>