DDR validation tools can't connect to server

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR validation tools can't connect to server

722 Views
sergiohernandez
Contributor I

Hello,

I'm trying to validate a custom board with a T2080 device.

From codewarrior I can connect to the board and I can access all registers of T2080 processor (LAW, IFC, DDR, ...)

But when I start QCVS in order to use DDR validation toos I get a error "can't connect to server!"

And when I open Validation tab no Target connection is available

pastedImage_1.png

I've a valid license for this product.

The CCS server  is working properly and detect CWTAP

Can tou help me?

thanks in advance.

0 Kudos
3 Replies

453 Views
addiyi
NXP Employee
NXP Employee

Make sure you select Target access to localhost not remote. Also, try creating a new target connection.

Adrian

0 Kudos

453 Views
sergiohernandez
Contributor I

Hello,

When I select localhost, automatically changes to remote.

I can’t generate a new target connection, the button is disabled.

De: addiyi

Enviado el: miércoles, 10 de mayo de 2017 12:53

Para: Hernández Sánchez, Sergio

Asunto: Re: - Re: DDR validation tools can't connect to server

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: DDR validation tools can't connect to server

reply from Adrian Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in CodeWarrior for QorIQ - View the full discussion<https://community.nxp.com/message/904078?commentID=904078&et=watches.email.thread#comment-904078>

0 Kudos

453 Views
addiyi
NXP Employee
NXP Employee

Try to use a new workspace. 

Adrian

0 Kudos