I am using CodeWarrior Power Architecture 10.1.1 and i have connected PSC9131RDB. Actually in CodeWarrior Power Architecture 10.1.1, PSC9131 is not mentioned in the list of supported devices. So I selected P1010 as it contains single e500 core. With that configuration, i am able to bulid successfully. Bt when i tried 2 debug, at the end of debug session following error is getting displayed :
Failed to resume target process., CCSProtocolPlugin : [CCS last error: USB open failure ]
How can i rectify this so that i can run my code on e500 core with PSC9131RDB using the IDE CodeWarrior Power Architecture 10.1.1?..
Please do not cross-post your questiuon into other forums.
---Tom