Cannot get CW for Coldfire 7.2 EVAL to run.   WHY?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Cannot get CW for Coldfire 7.2 EVAL to run.   WHY?

跳至解决方案
4,325 次查看
bmohat
Contributor I

    I have been able to get CW for ColdFire ver. 7.2 EVALUATION version to run on several PCs, but not on my main workstation PC.   The Installation seems to work fine (no errors are reported).   But when I try to run CodeWarrior, it starts to bring up the background of the IDE, then immediately "crashes".   Windows opens a dialog box that reports that:

 

           Integrated Development Environment has encountered a

           problem and needs to close.  We are sorry for the inconvenience.   (etc, etc.)

 

           And, this dialog box asks if I want to send a problem report to Microsoft or not.

 

 

    Now, this is the 30-day EVAL copy (I haven't loaded any "dongle drivers" or license files yet.)   The IDE just

won't run...it just blows away within 3 or 4 seconds after starting.

 

      Every PC I was able to get CW to run on was a uniprocessor PC.  My "workstation" PC is a Intel QUAD processor,

running XP Pro (32 bit).   Does CW not run on multi-core PCs?

 

      One other possibility:  my "workstation" PC has many programs on it that are managed by FlexLM.   Many of these programs are 10 years old or older, so there are many copies of FlexLM and lmgrd.xxx  in that PC.    Is it possible that lmgrd  might be fighting with older versions?   If so, how can I debug / fix this?   FlexLM is a DISASTER when trying to run many licensed programs on the same PC.   Can anyone help me with this>?

标签 (1)
标记 (1)
0 项奖励
1 解答
1,200 次查看
jonathang
Contributor II

I just wasted a couple of days tracking down something that sounds like the same problem:

 

Running CW for Coldfire 7.2 Special Edition on Windows XP pro.  It would crash every few minutes, giving me this in the event log:

 

Event Type: Error
Event Source: Application Error
Event Category: None
Event ID: 1000
Date:  5/8/2010
Time:  1:19:54 AM
User:  N/A
Computer: JCG-LAPTOP
Description:
Faulting application ide.exe, version 5.9.0.5293, faulting module lmgr11.dll, version 0.0.0.0, fault address 0x0007f841.

For more information, see Help and Support Center at http://go.microsoft.com/fwlink/events.asp.
Data:
0000: 41 70 70 6c 69 63 61 74   Applicat
0008: 69 6f 6e 20 46 61 69 6c   ion Fail
0010: 75 72 65 20 20 69 64 65   ure  ide
0018: 2e 65 78 65 20 35 2e 39   .exe 5.9
0020: 2e 30 2e 35 32 39 33 20   .0.5293
0028: 69 6e 20 6c 6d 67 72 31   in lmgr1
0030: 31 2e 64 6c 6c 20 30 2e   1.dll 0.
0038: 30 2e 30 2e 30 20 61 74   0.0.0 at
0040: 20 6f 66 66 73 65 74 20    offset
0048: 30 30 30 37 66 38 34 31   0007f841
0050: 0d 0a                     ..     

 

 

As you see, lmgr11.dll is fingered as the culprit.  It apparently woke up after perhaps minutes and blew up.  I determined that this only happened on a particular computer, and only if the project file resided on a particular disk partition.  Then I monitored file activity with filemon.exe, and learned that after 5 minutes or so, lmrg11.dll wakes up and scans the root directory of the partition that the project file is on.  It opens every file and directory in the root partition.

 

On the system in question, there is one file in the root directory that has a corrupted last-modification timestamp.  Windows Explorer shows a timestamp of Wednesday, November 24, 2094, 8:13:02 PM.  The os.stat() function in python returns a large negative number st_mtime=-353477714, which the various datetime functions refuse to parse.  I have no idea why this file is corrupted that way, but it has apparently been there for years.

 

When lmgr11.dll attempted to touch that file with the bad timestamp, it crashed.  Someone needs to feed this back to flexlm tech support.

 

My solution was easy enough -- I moved that file out of the root directory and will eventually update the timestamp once I'm done looking at this problem.  IAnyone experienceing a problem like this should look for a corrupted timestamp on a file somewhere on the disk partition.

 

This issue raises a couple of questions in my mind:

  1. Why is the flexlm lmgr11.dll license manager active in the Special Edition, where the software is freely downloadable and there are no license codes.
  2. Why is lmgr11.dll scanning my disk partititon every few minutes?  What is it looking for?  I see no evidence that it is trying to "phone home" with information snooped from my computer, and my firewall should warn me if it tried that, but this kind of activity tends to bring out the paranoia.

在原帖中查看解决方案

0 项奖励
9 回复数
1,200 次查看
ed_smith_mqx_le
Contributor III

Yes thanks for the post.  I ended up re-installing Windows from CD and that fixed the problem.  Still an issue in CW 10.6.  If you have a crash in file LMGR11.dll this is the problem to look for.

0 项奖励
1,200 次查看
Piotr
Contributor I

I have very similar problem on one of my workstations. It's uniprocessor, so I don't think number of CPUs matters. Error message points to lmgr11.dll file, which is some version of Flex license manager. I do not have any  lmgr*.dll  files other then included with CW 7.2

0 项奖励
1,200 次查看
bmohat
Contributor I

It appears that  lmgr11.dll   is what is blowing away, although I don't

know why.   While I have other programs in this PC that are protected by

FlexLM, none of them are running at the same time.  (I've checked;  no other

version of lmgrxx.xxx is running in the background).   So, why is lmgr11.dll

blowing up?   There doesn't seem to be any reason for it

 

Is there any way to test  lmgr11.dll  by itself?.

0 项奖励
1,201 次查看
jonathang
Contributor II

I just wasted a couple of days tracking down something that sounds like the same problem:

 

Running CW for Coldfire 7.2 Special Edition on Windows XP pro.  It would crash every few minutes, giving me this in the event log:

 

Event Type: Error
Event Source: Application Error
Event Category: None
Event ID: 1000
Date:  5/8/2010
Time:  1:19:54 AM
User:  N/A
Computer: JCG-LAPTOP
Description:
Faulting application ide.exe, version 5.9.0.5293, faulting module lmgr11.dll, version 0.0.0.0, fault address 0x0007f841.

For more information, see Help and Support Center at http://go.microsoft.com/fwlink/events.asp.
Data:
0000: 41 70 70 6c 69 63 61 74   Applicat
0008: 69 6f 6e 20 46 61 69 6c   ion Fail
0010: 75 72 65 20 20 69 64 65   ure  ide
0018: 2e 65 78 65 20 35 2e 39   .exe 5.9
0020: 2e 30 2e 35 32 39 33 20   .0.5293
0028: 69 6e 20 6c 6d 67 72 31   in lmgr1
0030: 31 2e 64 6c 6c 20 30 2e   1.dll 0.
0038: 30 2e 30 2e 30 20 61 74   0.0.0 at
0040: 20 6f 66 66 73 65 74 20    offset
0048: 30 30 30 37 66 38 34 31   0007f841
0050: 0d 0a                     ..     

 

 

As you see, lmgr11.dll is fingered as the culprit.  It apparently woke up after perhaps minutes and blew up.  I determined that this only happened on a particular computer, and only if the project file resided on a particular disk partition.  Then I monitored file activity with filemon.exe, and learned that after 5 minutes or so, lmrg11.dll wakes up and scans the root directory of the partition that the project file is on.  It opens every file and directory in the root partition.

 

On the system in question, there is one file in the root directory that has a corrupted last-modification timestamp.  Windows Explorer shows a timestamp of Wednesday, November 24, 2094, 8:13:02 PM.  The os.stat() function in python returns a large negative number st_mtime=-353477714, which the various datetime functions refuse to parse.  I have no idea why this file is corrupted that way, but it has apparently been there for years.

 

When lmgr11.dll attempted to touch that file with the bad timestamp, it crashed.  Someone needs to feed this back to flexlm tech support.

 

My solution was easy enough -- I moved that file out of the root directory and will eventually update the timestamp once I'm done looking at this problem.  IAnyone experienceing a problem like this should look for a corrupted timestamp on a file somewhere on the disk partition.

 

This issue raises a couple of questions in my mind:

  1. Why is the flexlm lmgr11.dll license manager active in the Special Edition, where the software is freely downloadable and there are no license codes.
  2. Why is lmgr11.dll scanning my disk partititon every few minutes?  What is it looking for?  I see no evidence that it is trying to "phone home" with information snooped from my computer, and my firewall should warn me if it tried that, but this kind of activity tends to bring out the paranoia.
0 项奖励
1,200 次查看
bowerymarc
Contributor V

thanks for the post, it's still very relevant.  I ran into this yesterday with CW 10.5 on win XP SP2.  My addition is that it could also be a file name issue.  I had my workspace on a drive shared with OSX (running CW in parallels), and the linker (which launches lmgr11.dll) was searching the root of the workspace drive, and found a name with parentheses in it and crashed.  Lmgr11.dll itself wasn't scanning the directories it was the parent.  So my advice, also look out for filenames (probably only relevant if you're on a non DOS/FAT32/NTFS drive).

0 项奖励
1,200 次查看
bmohat
Contributor I

   AH!   You're right!   lmgr11.dll   does apparently scan several directories for file dates

(to see if your 30-day evaluation period is over).   One place it goes is to c:\Windows .... and

it scans every file.   In my case, I had several files  with the name   (whatever).ocx ..... with the

file Type listed as  "ActiveX Control".   But, the file dates were not visible.    (See the attached

screenshot).   When I checked the "properties" of these files, they had file dates in the year 1617.

Nice.

 

    I downloaded a utility that allowed me to change file dates.  (And, you have to get them ALL....

including the file created date..... ALL dates have to be valid, and recent.   I'm assuming > 1980

or so.)   Once fixed up,   CodeWarrior works just fine.

 

  

    Thanks also for the tip about  filemon.exe.    I found that this functionality is included in

the "Process Monitor" from sysinternals.       http://www.sysinternals.com

 

To find files that cause  lmgr11.dll to choke:

1)  Download the process monitor, start it

2)  Start CodeWarrior.

3)  When lmgr11.dll  "crashes" .... look at the BOTTOM of the screen, to see

      the last files that lmgr11.dll was trying to open.   One of them will have a corrupt

      file date.

 

   I have reported this error to the CodeWarrior developers..... they will report it back

to Flexera, and try to get this "bug" cleaned up.

 

--Bill

 

0 项奖励
1,200 次查看
tagger
Contributor I

Great troubleshooting. I had 3 OCXs, all with numbered names and invalid dates. I did a registry search for all of them and they were not in the registry, so I am pretty sure they are not valid or used. They are much easier to archive than to change both the created and modified dates.

0 项奖励
1,200 次查看
DrTune
Contributor I

Niice thanks I just lost three working days to that one - the real joy is that you can uninstall+reinstall the whole f'ing eclipse package (wasting plenty of time) and it still screws you. 

 

For the record my problem was my machine started up one day thinking it was the year 2080 (dodgy clock battery), and I got the file

 

c:\Windows\PFRO.log

 

created by some regular windows (7) process, with a date in the year 2080.

 

I just deleted that, and yay, works again.  Of course now I lost three work days to another stupid compiler issue (also see "Linker silently corrupts INCBIN data" etc).

 

Grr.  You'd think there'd be a big sign somewhere to warn people of this issue wouldn't you? Hey maybe the license manager DLL gets less f'witted or perhaps just gets removed...

 

 

0 项奖励
1,200 次查看
Piotr
Contributor I

Congratulations, it seems you've found the source of the problem. I've check my workstation for files with strange datestamps and I've found nothing. Anyway, there was one file in C:/windows dated 1980-01-01 so  to be sure I changed this to 1981-01-01. And now CW7.2 starts flawlessly !

There is nothing malicious for the license manager to look for timestamps of various files on the disk, it tries to detect cases when calendar on the PC was set backwards. But I would prefer the software is tested before releasing it to the customers  :smileysad:

0 项奖励