When I follow the application note http://cache.nxp.com/files/soft_dev_tools/doc/app_note/AN5165.pdf?fsrch=1&sr=1&pageNum=1 to debug AIOP reflector source level application from CW4NETv2015.08.
CodeWarrior for APP Version: 10.1.1 Build Id:150805
Board used : LS2085RDB
I want to debug AIOP from system entry point referring to the section " 6 Debugging AIOP APP using CodeWarrior", with the following approach.
1: CW_APP Debug->Attach AIOP
2: CW_ARMv8 ->Inspect
3:CW-ARMv8 reset
4:CW_APP debugger shell bp __sys_start
5:CW_ARMv8->Resume
But AIOP sys_start breakpoint is not hitting
Please refer to section B given below and let me know what I may be missing.
Building AIOP:
Added dwarf symbolic info in meta-fsl-networking/recipes-dpaa2/aiop-refapp/aiop-refapp_git.bb.
::::::::::::::::::::::
DEPENDS = "aiopsl"
S = "${WORKDIR}/git/${BPN}"
inherit deploy
CFLAGS += "-sym dwarf-2, full"
LDFLAGS += "-sym dwarf-2, full"
SRC_URI = " \
::::::::::::::::::::::::
Build AIOP Reflector App
$bitbake aiop-refapp -c cleansstate
$bitbake aiop-refapp
Program AIOP Reflector Application ELF
tftp 0x80000000 ls2085-ear5/aiopapp/aiop_reflector.elf
erase 0x584900000 +$filesize
cp.b 0x80000000 0x584900000 $filesize
What could be the probable reason?
Hi Yiping,
I added some auxiliary steps to avoid using of the CW for ARMv8 (keeping just CW for APP) and the problem should disappear now. Please use the attached AN.
Also, I just bitbake -ed the application, not added/modified the recipe - please note that the debug symbols are added by default. Also, I recommend to build the app with CW and to set the optimization level to -O0 (Project Properties > C/C++ Build > Settings > Compiler > Optimization > Optimization Level 0)
Thank you,
Marius
Hello Marius,
I followed the application note shred by you with Codewarrior for APP 10.1.1 build 150805.
After enabling "Trace and Profice" in step 7, The "Upload Trace" Tab is disabled in my CW for APP.
What can be the reason ?
7. Collect hardware trace
Upload Trace tab is disabled
Thanks
Sanjay