USB-ML-12 for target MC9S12XDP in CodeWarrior 4.5 or 4.6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB-ML-12 for target MC9S12XDP in CodeWarrior 4.5 or 4.6?

跳至解决方案
2,356 次查看
Pang
Contributor I
Hi everyone,
 
Recently, I just purchased USB-ML-12 from P&E Micro. I am going to use it as a connection for debugging  in CodeWarrior V4.5/V4.6. I just install the drive for USB-ML-12. When I created a new project in Page 10,
 
I chose P&E MultiLink/Cyclone for connection. Do I still need to install any other debugger utilities from P&E Micro so that I can debug for my target MC9S12XDP in CodeWarrior?
 
Thanks,
 
Pang
 
 
 
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
869 次查看
J2MEJediMaster
Specialist I
You should be about ready. Try running the debugger (Project | Debug) and see if True-Time Simulator and Real-Time Debugger launches.

---Tom

在原帖中查看解决方案

0 项奖励
回复
3 回复数
870 次查看
J2MEJediMaster
Specialist I
You should be about ready. Try running the debugger (Project | Debug) and see if True-Time Simulator and Real-Time Debugger launches.

---Tom
0 项奖励
回复
869 次查看
Pang
Contributor I
I just tried and it was working!!!. Thanks a lot, Alban and Tom.
 
Pang
0 项奖励
回复
869 次查看
Alban
Senior Contributor II
Hi Pang,

No, you don't need anything else.
P&E utilities are bundled with CodeWarrior as standard.

Cheers,
Alban.

Message Edited by Alban on 2007-01-25 04:05 PM