Hi,
I am using codewarrior V10.7.
I have issue regarding target connection setting.
Sometimes it will not show target connection setting when i import existing project in CW workspace as below,
I am not getting why this is happening,is there any issue in codewarrior or issue in our project import setting or something else.
Request you to guide for the same.
Hello PRATIBHA SURABHI ,
You can add a debug connection interface into your project.
There is a document describe the steps in detail, please have a look at my attachment .
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello ,
You can also downlaod it from NXP website :
https://www.nxp.com/docs/en/application-note/AN4902.pdf?fsrch=1&sr=1&pageNum=1
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Alice_Yang
Thank you for the attachment.
Can you please tell me as to why the Connection in the Target Settings disappears sometimes?
Hello PRATIBHA SURABHI,
It seems when delete the .launch file , open the project again, the debug configration will disappeared.
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Alice_Yang,
Thank you.
Can you explain a situation or a a scenario where the above mentioned .launch files would get deleted?
I faced the problem of target connection missing when i imported the existing project.
How can the .launch files get deleted when importing a existing project?
Even I performed the same steps.
I directly import an existing project.
Also i tried by deleting the launch file(1 file).it ddint work
I tried after deleting the PEMICRO files (2 files ) such that the debugger folder was empty.
Still i was able to see a target setting.