Hi all,
i am using the TWR-K60F 120M Board. The processor is an ARM Cortex M4. I am trying to use Simulink to work with my Board. To develop a target in Simulink for my board, i need some informations.
1) Which toolchain can i use for my board (i think ARM GCC, is this right?).
2) I need the compiler and assambler flags, which will be used during the compilation and linking phase
3) I need a linker command file, which gives me information about the memory regions of the controller and which code will sit in which part of it.
Have someone any idea how i can get that informations?
Until today i only used CodeWarrior. There i did not need to know about the toolchain, compiler and assambler flags and the linker command file. But for Simulink i need that.
Best Regards
Armend
已解决! 转到解答。
Hi,
1 You can choose either ARM GCC or Freescale ARM compiler. But I recommend you use ARM GCC. You can select it with project wizard
2 Could you please specify what is “the compiler and assambler flags”?
3 Once you create a new project with wizard, you will see *.ld(ARM GCC) or *.lcf (Freescacle ARM) file under the project folder. This is the linker command line file.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
1 You can choose either ARM GCC or Freescale ARM compiler. But I recommend you use ARM GCC. You can select it with project wizard
2 Could you please specify what is “the compiler and assambler flags”?
3 Once you create a new project with wizard, you will see *.ld(ARM GCC) or *.lcf (Freescacle ARM) file under the project folder. This is the linker command line file.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jennie Zhang,
thank you for your help.
I am not sure what the compiler and assambler flags are, but i found something in the internet:
I have that from https://www.mikrocontroller.net/articles/ARM_GCC But it's in german.
As you can see i need the Information about -mcpu, -mfloat-abi, -mfpu and -mthumb (for Cortex M4).
Where can i look for that information in codewarrior.
Perhaps the following always applies:
But what about -mfloat-abi? It can be soft, softfp or hard.
Best Regards
Armend
Hi Amend.
if we create a new project with wizard, we can see -mfloat-abi can be:
each of above selection is for different library. for example, -mfloat-abi=hard is for this library:
we can check the project target processor here:
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------