Search/Find in File Crashes CW HC(s)08 v 5.7.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Search/Find in File Crashes CW HC(s)08 v 5.7.0

ソリューションへジャンプ
2,579件の閲覧回数
Maustin
Contributor I
Often when I use the search/find in files command in the "new improved" CW IDE the program crashes and of course loses everything since my last save (AAAARRRRG!)  This obviously is very annoying and never happened in the previous version (3.1).   Has anyone else had this problem?  Is there a service pack since that fixed this bug?  Should I junk the new version and re-install 3.1?
Thanks for the help!
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
610件の閲覧回数
marc_paquette
Contributor V
I'm not sure what could be causing this problem except for an obscure bug that prevented more than search using regular expressions.
 
I can only suggest that you send a bug report to find out more about this problem. To submit a service request:

1. Go to http://freescale.com/support

2. In the Develop column, click "Technical Support."

3. Click "Submit a service request."
 
Marc.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
611件の閲覧回数
marc_paquette
Contributor V
I'm not sure what could be causing this problem except for an obscure bug that prevented more than search using regular expressions.
 
I can only suggest that you send a bug report to find out more about this problem. To submit a service request:

1. Go to http://freescale.com/support

2. In the Develop column, click "Technical Support."

3. Click "Submit a service request."
 
Marc.
0 件の賞賛
返信
610件の閲覧回数
pittbull
Contributor III
Hi,
I have an old CodeWarrior for HCS12 which also crashes in "Find in Files" (Don't know the version number). But that's not a problem for me. I never use this "feature" :smileywink:. I use this instead: http://desktop.yahoo.com/
0 件の賞賛
返信