Hello,
I am getting error on ending line of a function (at closing curly brace).
Here's my error:
<fileName>.c|1677|0|1|91472|1)
=}
>internal compiler error (report to <cw_bug@freescale.com>)
>while executing in file 'ExpandIR.c' line: 7135
>(compiling '<functionName>' in '<fileName>.c')
Errors caused tool to abort.
NMAKE : fatal error U1077: '"C:\Freescale\CW MCU v11.1\MCU\S12lisa_Tools\Build_Tools\mwccs12lisa.exe"'
: return code '0x1'
Stop.
NMAKE : fatal error U1077: 'C:\apps\Nmake\nmake.EXE' : return code '0x2'
Stop.
Usually compiler lay out their concerns for our code. But this one just tells line no.! Installed it today.
P.S: I emptied out function, the error vanished.
Also, I changed compiler optimization level from 2 to 0, it worked. No error. Any opt level except 0 generates error.
P.S: I am using evaluation version of compiler (awaiting license from customer). Is this error because of any free eval limit?
Thanks
bump!
anyone?