Using Codewarrior 6.3. I can put a lookup table in RAM, but cannot seem to figure out the syntax to place it in ROM or flash memory. Tried using extern, but then it seems the table is placed in ram and flash. For placing the table in ram, I have this in the header along with the table values:
static const unsigned char temperature[250] = { ... };
Works fine in ram.
I tried this to get the table in flash:
In the header:
extern unsigned char temperature[250];
then in the code:
extern unsigned char temperature[44] = { ...};
This places the table in both ram and flash!
What is the correct syntax to place a table in flash?
Thank you!
解決済! 解決策の投稿を見る。
Hi Tom
You can allocate a constant variable at an absolute address using the @ modifier.
For example allocating a constant called VersionNbr at address 0xF000 and initializing it to 2 is done as follows:
const int VersionNbr @0xF000 = 2;
Same notation can be used for a constant string as follows
const char VersionStr[] @0xF000 ="Version 4.6";
if you don't use @, CW will allocate const variable to default const section automatically.
If this version number is not used anywhere in the application, you have to instruct the Linker to link it to the application even though it is not used.
This is done specifying the constant name in the .prm file ENTRIES block.
For example:
ENTRIES
VersionNbr VersionStr
END
Last, please enable –Cc option in Compiler option setting panel.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you Jun! Your solution saved me so much time! Can you please provide a link to the document that has this information? Thank you!
Hi Tom
You can allocate a constant variable at an absolute address using the @ modifier.
For example allocating a constant called VersionNbr at address 0xF000 and initializing it to 2 is done as follows:
const int VersionNbr @0xF000 = 2;
Same notation can be used for a constant string as follows
const char VersionStr[] @0xF000 ="Version 4.6";
if you don't use @, CW will allocate const variable to default const section automatically.
If this version number is not used anywhere in the application, you have to instruct the Linker to link it to the application even though it is not used.
This is done specifying the constant name in the .prm file ENTRIES block.
For example:
ENTRIES
VersionNbr VersionStr
END
Last, please enable –Cc option in Compiler option setting panel.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------