Need peripheral driver library for ColdFire MCF52233 with CodeWarrior 10.7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need peripheral driver library for ColdFire MCF52233 with CodeWarrior 10.7

1,020 Views
muhibraza
Contributor I

Hi,

I am looking for a standard peripheral driver library that has all the C files and the H files with typical usage examples for the Coldfire v2 ethernet controller MCF52233. My IDE is CodeWarrior 10.7 but I couldnt find these files in the install directory or the website itself. Does any one have something like this?

Labels (1)
0 Kudos
Reply
1 Reply

681 Views
miduo
NXP Employee
NXP Employee

Hi,

Please be note that the M52233DEMO board is quite old and all sample code/driver were developed under CW 7.x.We don't have demo example based on MCU V10.7 for this board. Now Processor Expert is included in the tool.
So for your case, if you really need to use the CW 10.x with the M52233DEMO, I would recommend you may use the CW 10.1, which has the M52233DEMO included.

0 Kudos
Reply