MC9S08PL16SCTG Processor Missing at Codewarrior V11.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC9S08PL16SCTG Processor Missing at Codewarrior V11.1

跳至解决方案
2,811 次查看
egoitztoledo
Contributor III

I am traying to create a new bareboard proyect for a MC9S08PL16SCTG but I am having some troubles. I have installed the "CodeWarrior MCU 11.1 Service Pack for S08PB and S08PLS" service pack, so now, I can see the micro at the Devices list for sellection. The first problem is that at the new project assistant, the "Rapid Application Development" (image attached) step does not appear, so I can't create the project where I will be using Procesor Expert.

Furthermore, at the "Components" the processor is missing, so definetly, there is I have no way to use Processor Expert.

I wonder if these problems I am facing is a "bug" that will be solved or an intended thing. If so, I have never made a project without Processor Expert, so I would appreciate a guide or so to carri it out.

0 项奖励
回复
1 解答
2,802 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry the MC9S08PL family does not have a Processor expert  option

I really sorry

Regards

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,810 次查看
egoitztoledo
Contributor III

By the way...Hello and thank you in advance.

Sorry for the oversight.

0 项奖励
回复
2,803 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry the MC9S08PL family does not have a Processor expert  option

I really sorry

Regards

0 项奖励
回复
2,794 次查看
egoitztoledo
Contributor III

Hi Vicente, thank you for your answer.

It's a pitty, because as I said, I have never made a project whithout PE and I don't know how could I do it...

Dou you know if it will exist the option in a short period?

Regards.

0 项奖励
回复
2,788 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

You can create a PE project for the PA family, check the configurations and copy them to a new project (without PE) for the PL

 

Sorry, but this is the only option that I have in mind

 

Regards

 

0 项奖励
回复
2,774 次查看
egoitztoledo
Contributor III

OK, thank you for your answers.

Best regards.

0 项奖励
回复