LIST-File on CW5.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LIST-File on CW5.1

3,072 次查看
Truk
Contributor I
I try to setup CW5.1 to make a .LST file but I could not find where I could do this. The HELP tell me to add the -L option but where can I do this? I have only the MAKE button which does all, but I can't find the file behind this button to modify nor menue where I could setup the Make file.
 
thanks for any help
Truk
 
标签 (1)
标记 (1)
0 项奖励
回复
7 回复数

885 次查看
J2MEJediMaster
Specialist I
The listing file is generated by the assembler. If you're using the IDE, go to the project's Preferences panel (Edit | YourProjectNameHere Settings...) and choose the Assembler panel. You might be presented with a command line in which case, try:

-L=%(TEXTPATH)\%n.lst

Or, if there's a GUI, try checkboxing the item, Generate a Listing File.

---Tom
0 项奖励
回复

885 次查看
swright
Contributor I

I too am trying to get the assembler to produce a listing file.

I went to the Edit->YourProjectNameHere Settings and using the GUI, I select Target Settings Panel->ColdFire Assembler but the Generate Listing File checkbox is grayed out!

Is this a limitation of the special edition version of CodeWarrior for ColdFire V6.3 build 14 or simply a bug?

 

 

0 项奖励
回复

885 次查看
CrasyCat
Specialist III

Hello

For CodeWarrior for Coldfire to get a listing file for a specific source file:

  - Select the source file in the .mcp window
  - Click on it with the right mouse button
  - Select Disassemble from the drop down menu.

A new editor window should show up showing the disassembly listing.

You can adjust the content of the listing file using the "ELF Disassembler" panel.

I hope this help.

CrasyCat

0 项奖励
回复

885 次查看
swright
Contributor I

hmmm...

I've looked at the disassembly function but it doesn't produce a standard assembly listing file.

 

Is there any way to invoke the assembler from a command line and, if so,  are there other options  available?

 

Scott

 

0 项奖励
回复

885 次查看
CrasyCat
Specialist III
Hello
I do not know what you call a "standard assembly listing file"? Can you tell me what you expect.
 
Anyway, you can produce a disassembly listing file using the command line compiler and specifying option
-dis.
The command line compiler can be found in {Install}\E68K_Tools\Command_Line_Tools and is called mwccmcf.exe.
 
I am afraid this will probably generate the same disassembly listing as the disassemble menu.
There is no separate tool available to disassemble an object file.
 
CrasyCat
0 项奖励
回复

885 次查看
swright
Contributor I

Code:

 Assembly Source File Fragment_INIT_MBUS:;_READ_TEMPERATURE:        CLR.B        MBSR(A5)       ;CLEAR STATUS REGISTER        MOVEQ        #$13,D0        ;DIVIDE 40MHz BY 480 = 83K33                                    ;DIVIDE 54MHz BY 480 = 112K5        MOVE.B       D0,MFDR(A5)        CLR.B        MBCR(A5)       ;RESET AND DISABLED        MOVEQ        #$80,D0        MOVE.B       D0,MBCR(A5)    ;ENABLE M-BUS        MOVEQ        #$A5,D0        ;ARBITRARY MASTER ADDRESS        MOVE.B       D0,MADR(A5)    ;SET ADDRESS        BSR.W        _TX_A_W        ;TRANSMIT ADDRESS:WRITE        BNE.W        NO_ACK         ;ERROR                'Standard' Assembly Listing File  00000000 03            51 _INIT_MBUS:  00000000 03            52 ;_READ_TEMPERATURE:  00000000 03 422d 01ec  53         CLR.B        MBSR(A5)       ;CLEAR STATUS REGISTER  00000004 03 7013       54         MOVEQ        #$13,D0        ;DIVIDE 40MHz BY 480 = 83K33  00000006 03            55                                     ;DIVIDE 54MHz BY 480 = 112K5  00000006 03 1b40 01e4  56         MOVE.B       D0,MFDR(A5)  0000000a 03 422d 01e8  57         CLR.B        MBCR(A5)       ;RESET AND DISABLED  0000000e 03 7080       58         MOVEQ        #$80,D0  00000010 03 1b40 01e8  59         MOVE.B       D0,MBCR(A5)   ;ENABLE M-BUS  00000014 03 70a5       60         MOVEQ        #$A5,D0        ;ARBITRARY MASTER ADDRESS  00000016 03 1b40 01e0  61         MOVE.B       D0,MADR(A5)   ;SET ADDRESS  0000001a 03 6100 00ca  62         BSR.W        _TX_A_W        ;TRANSMIT ADDRESS:WRITE  0000001e 03 6600 00b6  63         BNE.W        NO_ACK         ;ERROR                CodeWarrior's Dis-assembly FileAddress     ObjectCode        Label  Opcode   Operands              Comment0x00000000                    _INIT_MBUS:;                             INIT_MBUS:0x00000000                    __start:;                             _start:0x00000000                    _start:;                             start:0x00000000  0x422D01EC               clr.b    492(a5)0x00000004  0x7013                   moveq    #19,d00x00000006  0x1B4001E4               move.b   d0,484(a5)0x0000000A  0x422D01E8               clr.b    488(a5)0x0000000E  0x7080                   moveq    #-128,d00x00000010  0x1B4001E8               move.b   d0,488(a5)0x00000014  0x70A5                   moveq    #-91,d00x00000016  0x1B4001E0               move.b   d0,480(a5)0x0000001A  0x610000CA               bsr.w    *+204                 ; 0x000000e60x0000001E  0x660000B6               bne.w    *+184                 ; 0x000000d6


 
The above is an example of assembly code, listing file and disassembly.  Note that the disassembly loses the source comments and operand labeling, making it less than useful.

I gather that not too many of your users have as much legacy code written in assembler as I have.  I need to carry this old code up into an environment supporting the c, c++, ethernet stacks, etc.  I'm sure I'll be porting this legacy code over time as needed, but for now, if it ain't broke....

Thanks anyways,

Scott

 

 

 

0 项奖励
回复

885 次查看
CrasyCat
Specialist III

Hello

You will not get exactly the output you are use to.
But if in the ELF disassembler panel you make sure "Show Source Code" and "Show Comments" are checked you get something as follows, which at least provides you with the comments and labels from the original source file.

Code:

;  105: asm_startmeup: ;  106: _asm_startmeup: ;  107:  ;  108:  move.w  #0x2700,SR ;0x00000000                    _asm_startmeup:;                             asm_startmeup:0x00000000                    asm_startmeup:0x00000000  0x46FC2700               move     #9984,sr;;  109:  move.l      #VECTOR_TABLE,d0 ;0x00000004  0x203C00000000           move.l   #VECTOR_TABLE,d0;;  110:  movec       d0,VBR ;  111:  ;  112:  /*  ;  113:   * At power-on reset, the initial PC must be between 0-4K so that  ;  114:   * CS0 will assert for accesses to Flash.  At this point, we need to ;  115:   * clear the CS0 address mask and change the PC to the real Flash  ;  116:   * location of 0xFFE00000.  This must be done before any branch or ;  117:   * jump instruction is executed! ;  118:   */ ;  119:  ;  120: /* This is a ROM target, so we are always running in ROM ;  121:     tst.l  #___Running_in_ROM ;  122:  beq   new_addr ;  123: */ ;0x0000000A  0x4E7B0801               movec    d,vbr;;  124:     bra   new_addr ;0x0000000E  0x60000024               bra.w    *+38                  ; 0x00000034;;  125:   move.l  #IMMaddr+1,d ;0x00000012  0x203C10000001           move.l   #268435457,d0         ; '....';;  126:  myopic   d,MBAR ;0x00000018  0x4E7B0C0F               movec    d,mbar;;  127:  move.l  #IMMaddr,a0 ;0x0000001C  0x207C10000000           movea.l  #268435456,a0         ; '....';;  128:  move.l  #0x20,d ;0x00000022  0x203C00000020           move.l   #32,d0                ; '... ';;  129:  move.l  d,$44(a0) ;0x00000028  0x21400044               move.l   d,68(a0);;  130:  nop ;0x0000002C  0x4E71                   nop      ;;  131:  jmp   new_addr   ;  132:  ;  133: new_addr: ;0x0000002E  0x4EF900000034           jmp      .text+104


 
Note that I get that with CodeWarrior Coldfire V6.x. I am not sure CodeWarrior for Coldfire V5.x has the same options available in the ELF Disassembler panel.

CrasyCat

0 项奖励
回复