PLEASE HELP!!!
I am extremely frustrated. I'm a student who's professor doesn't care to teach us how to do this. I have been unable to display to the 8x2 lcd screen included with the PBMCUSLK AXM-0392 REV D Development board. i'm using axiom's CSMB12 daughter board. the microcontroller is the MC9S12DT256MFUE.
From what i've discovered so far:
The lcd uses the SPI interface. It is driven by a serial to parallel shift register 74HC595D. It requires that the LCD_EN jumpers be installed and the SS_SEL Jumper to be connecting SS* instead of GPIO. Axioms CSMB12 board labels the MOSI0,MISO0,SCK0,and SS0 as PM<#> which leads one to believe that it is connected to Port M, but the microcontroller datasheet shows these connecting to Port S.
I set up the registers and used some example code from my text to try and write a character to the lcd screen.
void main{
// Initialize the spi interface
openspi0(void);
putcspi0('H');
delay1ms(1);}
/* please make sure that you never leave main */
}
//Here is the function to set up the spi registers.
void openspi0(void){
SPI0BR = 0x10; // set baud rate
SPI0CR1 = 0x50; // enable SPI, data shift on SCK’s rising edge, master mode
SPI0CR2 = 0x02; // disable bidirectional mode, SPI stops in wait mode
WOMS = 0x00; // enable Port S pull-up
DDRS = 0xE2;
}
// Function to desplay a character.
void putcspi0 (char cx){
char temp;
while(!(SPI0SR & 0x20)); // wait until write is permissible
SPI0DR = cx; // output the byte to the SPI
while(!(SPI0SR & 0x80)); // wait until write operation is complete
temp = SPI0DR; // clear the SPIF flag
}
Thanks in advance for the help!
Hello,
This problem is more complex than simply initialising the SPI module, and writing byte values to the shift register.
You will need to ascertain the hardware configuration before you will be able to write the code. For this you will need the schematic. Have you checked whether Axiom publish any LCD driver code for their board?
Regards,
Mac
Ouch, why did the prof have to go ahead and start off with a SPI based LCD? I mean, I know the LCD itself is parrallel, but the addition of the shift register makes life more difficult than it should be!
Oh, think I found it. You didn't actually enable the SPI to begin with, Lol:
You have:
SPI0CR1 = 0x50
Probably should be:
SPI0CR1 = 0xD0
Since SPI0CR1 bit 7 is the SPIE bit...
By the way, do you have a copy of the device manual?
Edit: Doh, read the register map wrong.
I'd like to add that when debugging, the program stops at "while(!(SPI0SR & 0x80))" within the putcspi0 function. This is checking a flag in the status register to see if the data transfer is complete. this flag never clears.
craigc, after going through the 74HC595D data sheet, my diagnosis is "what the heck?"
The operation you currently have is waiting on input from the shift register... but after consulting the datasheet I see no way how that would be possible.
Try omitting the while( !(SPI0SR & 0x80) ) line and see if anything happens.
AirDragon,
no, operation is waiting for transfer complete. How many bits is clocked out, so meny bits is clocked in. In master SPIF flag is set after transfer is complete (both out and in). Of course to make it working as transfer complete flag, you need to clear SPIF after each transfer by reading status reg followed by read of data reg. Craifgc's code looks well.
Craigc,
I don't know how old is your board and how faulty is MCU on it. It makes sense to check erratas.
Also could you verify if MODF flag is set or clear? It shouldn't be set, but somewhen long time ago (don't remember on which of HC11/HC12D or maybe S12D64) I saw MODF set after enabling SPI in master mode, which prevented switching to master mode. Solution was to read status reg before writing to SPICR1. This is normal sequence to clear MODF flag.