L1100 linker errors with CodeWarrior HC12 toolchain

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

L1100 linker errors with CodeWarrior HC12 toolchain

跳至解决方案
3,464 次查看
svenny29
Contributor I
Hi all!

I'm using the CodeWarrior HC12 toolchain V5.0.28 Build 5073. My project is based on standard software modules from different companies, so I can't change the source code. One software module is using a microcontroller register definition file for the MC9S12XDP512 (called Reg_xdp512.h). This file doesn't suit my needs (too few or missing bit and mask definitions etc.) and I want to use "mc9s12xdp512.h" from _CODEWARRIOR_DIR_\lib\hc12c\include.

As soon, as I include this file in my sources, I get the following warnings:

WARNING L1100: Segments .absSeg0 (0x0) and .absSeg652 (0x0) overlap
WARNING L1100: Segments .absSeg652 (0x0) and .absSeg1168 (0x0) overlap
WARNING L1100: Segments .absSeg1168 (0x0) and .absSeg1820 (0x0) overlap
WARNING L1100: Segments .absSeg1820 (0x0) and .absSeg653 (0x1) overlap
WARNING L1100: Segments .absSeg1 (0x2) and .absSeg654 (0x2) overlap
WARNING L1100: Segments .absSeg654 (0x2) and .absSeg1169 (0x2) overlap
WARNING L1100: Segments .absSeg1169 (0x2) and .absSeg1821 (0x2) overlap
WARNING L1100: Segments .absSeg1821 (0x2) and .absSeg655 (0x3) overlap
WARNING L1100: Segments .absSeg2 (0x4) and .absSeg656 (0x4) overlap
WARNING L1100: Segments .absSeg656 (0x4) and .absSeg1170 (0x4) overlap
WARNING L1100: Segments .absSeg1170 (0x4) and .absSeg1822 (0x4) overlap
WARNING L1100: Segments .absSeg1822 (0x4) and .absSeg657 (0x5) overlap
WARNING L1100: Segments .absSeg3 (0x6) and .absSeg658 (0x6) overlap
WARNING L1100: Segments .absSeg658 (0x6) and .absSeg1171 (0x6) overlap
WARNING L1100: Segments .absSeg1171 (0x6) and .absSeg1823 (0x6) overlap
WARNING L1100: Segments .absSeg1823 (0x6) and .absSeg659 (0x7) overlap
WARNING L1100: Segments .absSeg4 (0x8) and .absSeg660 (0x8) overlap
WARNING L1100: Segments .absSeg660 (0x8) and .absSeg1172 (0x8) overlap
WARNING L1100: Segments .absSeg1172 (0x8) and .absSeg1824 (0x8) overlap
WARNING L1100: Segments .absSeg5 (0x9) and .absSeg661 (0x9) overlap
WARNING L1100: Segments .absSeg661 (0x9) and .absSeg1173 (0x9) overlap
WARNING L1100: Segments .absSeg1173 (0x9) and .absSeg1825 (0x9) overlap
WARNING L1100: Segments .absSeg6 (0xA) and .absSeg662 (0xA) overlap
WARNING L1100: Segments .absSeg662 (0xA) and .absSeg1174 (0xA) overlap
WARNING L1100: Segments .absSeg1174 (0xA) and .absSeg1826 (0xA) overlap
WARNING L1100: Segments .absSeg7 (0xB) and .absSeg663 (0xB) overlap
WARNING L1100: Segments .absSeg663 (0xB) and .absSeg1175 (0xB) overlap
WARNING L1100: Segments .absSeg1175 (0xB) and .absSeg1827 (0xB) overlap
WARNING L1100: Segments .absSeg8 (0xC) and .absSeg664 (0xC) overlap
WARNING L1100: Segments .absSeg664 (0xC) and .absSeg1176 (0xC) overlap
WARNING L1100: Segments .absSeg1176 (0xC) and .absSeg1828 (0xC) overlap
WARNING L1100: Segments .absSeg9 (0xD) and .absSeg665 (0xD) overlap
WARNING L1100: Segments .absSeg665 (0xD) and .absSeg1177 (0xD) overlap
WARNING L1100: Segments .absSeg1177 (0xD) and .absSeg1829 (0xD) overlap
WARNING L1100: Segments .absSeg10 (0x10) and .absSeg668 (0x10) overlap
WARNING L1100: Segments .absSeg668 (0x10) and .absSeg1178 (0x10) overlap
WARNING L1100: Segments .absSeg1178 (0x10) and .absSeg1830 (0x10) overlap
WARNING L1100: Segments .absSeg11 (0x12) and .absSeg669 (0x12) overlap
WARNING L1100: Segments .absSeg669 (0x12) and .absSeg1179 (0x12) overlap
WARNING L1100: Segments .absSeg1179 (0x12) and .absSeg1831 (0x12) overlap
WARNING L1100: Segments .absSeg12 (0x13) and .absSeg670 (0x13) overlap
WARNING L1100: Segments .absSeg670 (0x13) and .absSeg1180 (0x13) overlap
WARNING L1100: Segments .absSeg1180 (0x13) and .absSeg1832 (0x13) overlap
WARNING L1100: Segments .absSeg13 (0x16) and .absSeg672 (0x16) overlap
WARNING L1100: Segments .absSeg672 (0x16) and .absSeg1181 (0x16) overlap
WARNING L1100: Segments .absSeg1181 (0x16) and .absSeg1833 (0x16) overlap
WARNING L1100: Segments .absSeg14 (0x17) and .absSeg673 (0x17) overlap
WARNING L1100: Segments .absSeg673 (0x17) and .absSeg1182 (0x17) overlap
WARNING L1100: Segments .absSeg1182 (0x17) and .absSeg1834 (0x17) overlap
WARNING L1100: Segments .absSeg15 (0x1A) and .absSeg675 (0x1A) overlap
INFORMATION L2: Message overflow, skipping WARNING messages



Before I added the linker option "-WmsgSw1100" these warnings were errors! As I don't like to see/get these warnings/errors everytime
I compile my project, I would like to fix it, but I don't know how:
I can't change the software module which is including the other definition file and I want to use "my own" favorite register definition file.

Is there any way to get rid of these warnings (without turning this warning off)?

Thanks for your help!
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,839 次查看
J2MEJediMaster
Specialist I
I've seen this slew of errors when I use the CodeWarrior project wizard to build the HC12 version of OSEK. OSEK provides its own HC12 header information. Those files, along with the standard boiler-plate headers the CodeWarrior project provides, create redundant definitions. What you are seeing is the linker complaining of these redundant definitions.

You're either going to have to live with the other software's header files, or carefully edit the CodeWarrior header file to include only the information that the other header files lack.

---Tom

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,840 次查看
J2MEJediMaster
Specialist I
I've seen this slew of errors when I use the CodeWarrior project wizard to build the HC12 version of OSEK. OSEK provides its own HC12 header information. Those files, along with the standard boiler-plate headers the CodeWarrior project provides, create redundant definitions. What you are seeing is the linker complaining of these redundant definitions.

You're either going to have to live with the other software's header files, or carefully edit the CodeWarrior header file to include only the information that the other header files lack.

---Tom
0 项奖励
回复