I can't install svn on codewarrior 11

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I can't install svn on codewarrior 11

509件の閲覧回数
shellingford
Contributor I

when I add new software,it is has problems:

Cannot complete the install because one or more required items could not be found.
  Software currently installed: CodeWarrior MQX 4.1 Plug-ins for ARM architecture (requires ARM architecture to be installed) 1.4.1.201408201355 (com.freescale.mqx.v4.1.arm.feature.group 1.4.1.201408201355)
  Missing requirement: CodeWarrior MQX 4.1 Plug-ins for ARM architecture (requires ARM architecture to be installed) 1.4.1.201408201355 (com.freescale.mqx.v4.1.arm.feature.group 1.4.1.201408201355) requires 'com.freescale.kinetis.architecture [1.0.0,2.0.0]' but it could not be found

when I check updates,it also has problems:

Cannot complete the install because one or more required items could not be found.
  Software currently installed: CodeWarrior MQX 4.0.x Plug-ins for ColdFire architecture (requires ColdFire architecture to be installed) 1.4.1.201401301129 (com.freescale.mqx.v4.0.cf.feature.group 1.4.1.201401301129)
  Missing requirement: CodeWarrior MQX 4.0.x Plug-ins for ColdFire architecture (requires ColdFire architecture to be installed) 1.4.1.201401301129 (com.freescale.mqx.v4.0.cf.feature.group 1.4.1.201401301129) requires 'com.freescale.coldfire.architecture [1.0.0,2.0.0]' but it could not be found

タグ(2)
0 件の賞賛
1 返信

360件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Shelling Ford,

Those errors does not seem to be related with SVN, those errors mention that the MQX plugin needs the Coldfire and Kinetis support to be installed on your CodeWarrior.

About installing SVN, you could use the following post as reference:

https://community.nxp.com/docs/DOC-329889 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛