Hi,
I am using the Codewarrior compiler in which i uses the both assembly and C code in a function. This is for HCS08 SG16 micro. I am facing an error like
Warning : C1404: Return expected in my function as below,
BYTE Get_IMask_Status(void)
{
#asm
tpa ; Read contents of CCR to A
and #0x08 ; isolate I mask bit
asla ; shift left by one bit
nsa ; nibble swap, Acc has the content of I bit
#endasm
}
I have the above function which retruns a BYTE, but i am reading that BYTE value from the Accumalator from the assembly code . but CW is throwing a error that return expected. But i am have not written the return statement in the C function but evenm though i am getting return indirectly from the A which is in assembly. is ther any way that i can remove this warning? Or how can i get the Accumulator value into C retun true.
Please reply to me.
解決済! 解決策の投稿を見る。
In order to disable message C1404 for a specific function (you would not want to do that for the whole compilation unit), you need to use #pragma MESSAGE with that function:
- pragma before the function, to disable the message
- pragma after the function, to set the message back to Warning again (so as to make sure that, were there other functions which miss the return statement, the warning will actually be reported for those functions).
Given your function, this means:
#pragma MESSAGE DISABLE C1404
BYTE Get_IMask_Status(void)
{
#asm
tpa ; Read contents of CCR to A
and #0x08 ; isolate I mask bit
asla ; shift left by one bit
nsa ; nibble swap, Acc has the content of I bit
#endasm
}
#pragma MESSAGE WARNING C1404
Hello,
The compiler does not analyse the actions of the assembly code, so it does not take into account that you are already returning the required value in the accumulator. To avoid the warning, you need to create a local variable, assign the accumulator value to the variable, and return the variable. Of course this reduces the efficiency of the code.
byte Get_IMask_Status(void){ byte temp; #asm tpa ; Read contents of CCR to A and #0x08 ; isolate I mask bit asla ; shift left by one bit nsa ; nibble swap, Acc has the content of I bit sta temp; #endasm return temp;}
This results in the following assembly code for the sub-routine. The additional code associated with the variable is indicated. The routine occupies eleven bytes.
.
pshh
tpa
and #0x08
lsla
nsa
tsx
sta ,x
lda ,x
pulh
rts
.
Here is an alternative version of the function, requiring nine bytes of code.
byte Get_IMask_Status(void){ byte temp = 0; __asm bmc B1; temp++; __asm B1: return temp;}
However, you do not need to use either of these functions to return the I-bit status. An intrinsic function is already available to do this, and requires smaller code. The function prototype can be found within the file <intrinsics_hc08.h>, present in the CW installation.
char __isflag_int_enabled( void);
Functions to return other status bits may also be of interest.
Regards,
Mac
Thanks for your good idea. I have to try out this new code implmentation. But i have to minimize the code size as we have critical flash requirements. I can go for the Message disable option. Again thanks for this new idea. I will try it out and come back to you...
Instead of using
#pragma MESSAGE WARNING C1404
in order to reset the message back to a warning you could use as well
#pragma MESSAGE DEFAULT C1404
That way you do not need to 'know' that it was a warning message.
BK
In order to disable message C1404 for a specific function (you would not want to do that for the whole compilation unit), you need to use #pragma MESSAGE with that function:
- pragma before the function, to disable the message
- pragma after the function, to set the message back to Warning again (so as to make sure that, were there other functions which miss the return statement, the warning will actually be reported for those functions).
Given your function, this means:
#pragma MESSAGE DISABLE C1404
BYTE Get_IMask_Status(void)
{
#asm
tpa ; Read contents of CCR to A
and #0x08 ; isolate I mask bit
asla ; shift left by one bit
nsa ; nibble swap, Acc has the content of I bit
#endasm
}
#pragma MESSAGE WARNING C1404
Thanks and it is working fine for me.