Hi,
I want to develop a tool which can parse the .MAP file of CodeWarrior project, and then automatically generate another file to store gobal variables name and their corresponding address.
Using CodeWarrior 5.x, there is a detailed description about gobal variables name and their corresponding address in .map file of S12x project.
But the .MAP files vary from CodeWarrior 5.x to CodeWarrior 2.x, there is no description about variables in .MAP file of CodeWarrior 2.x.
Could you tell me how i can obtain address and name of gobal variable in .MAP/.elf/.mot file of CodeWarrior 2.x project ?
Hi wang heng,
It might be quite challenging to get this info from map file.
What about disassemble your .elf file using CodeWarrior linker and extract all data section names that are writable during execution (Flags have bit 0x01 set):
e.g.:
==> .sdata [13]: Section Header
type: 00000001, flags: 00000003
address: 00030800, offset: 00001800, size: 0000000c
link: 00000000, info: 00000000, alignment: 8, entry size: 0
==> .sdata2 [14]: Section Header
type: 00000001, flags: 00000002
address: 00030810, offset: 00001810, size: 00000004
link: 00000000, info: 00000000, alignment: 8, entry size: 0
==> .bss [15]: Section Header
type: 00000008, flags: 00000003
address: 400004e8, offset: 00001818, size: 0000000c
link: 00000000, info: 00000000, alignment: 8, entry size: 0
and then filter symbol table ".symtab" bind = GLOB; type = OBJ; for only sections (shdnx) extracted in the previous step
e.g.
==> .symtab
entry spndx value size bind type other shndx name
[ 0] 0 00000000 0 LOC (00) NULL(00) 00 (0000)UND
[ 1] 1 00000000 0 LOC (00) FILE(04) 00 (fff1)ABS main.c
[ 2] 0 00030000 0 LOC (00) SECT(03) 00 (0006).text_vle .text_vle
[ 3] 0 0003041c 0 LOC (00) SECT(03) 00 (000a)extab extab
[ 4] 0 0003044c 0 LOC (00) SECT(03) 00 (000b)extabindex extabindex
[ 5] 0 400004d0 0 LOC (00) SECT(03) 00 (000d).sdata .sdata
[ 6] 0 400004e0 0 LOC (00) SECT(03) 00 (000e).sdata2 .sdata2
[ 7] 8 0003041c 8 LOC (00) OBJ (01) 00 (000a)extab @256
[ 8] 13 0003044c 12 LOC (00) OBJ (01) 00 (000b)extabindex @257
[ 9] 18 00030424 8 LOC (00) OBJ (01) 00 (000a)extab @278
[ 10] 23 00030458 12 LOC (00) OBJ (01) 00 (000b)extabindex @279
[ 11] 28 0003042c 8 LOC (00) OBJ (01) 00 (000a)extab @296
[ 12] 33 00030464 12 LOC (00) OBJ (01) 00 (000b)extabindex @297
[ 13] 38 00030434 8 LOC (00) OBJ (01) 00 (000a)extab @306
[ 14] 43 00030470 12 LOC (00) OBJ (01) 00 (000b)extabindex @307
...
[ 73] 366 400004d0 4 GLOB(01) OBJ (01) 00 (000d).sdata myGlob
[ 74] 373 400004e0 4 GLOB(01) OBJ (01) 00 (000e).sdata2 myConst
[ 75] 381 000300ea 102 GLOB(01) FUNC(02) 00 (0006).text_vle clear_CF
...
You could possibly use the command line GNU utility - readelf to get this information.
Hope it helps.
Stan