I just started up my working CW10.5 and it said that there were updates available. So I installed them. I also installed the new Windows updates at the same time. Now CW won't start up, it crashes out pointing to an error log.
I usually use CW10.2 on Linux, but just a week ago I decided to try CW10.5 on Windows. Hmmmm......
I'm wondering if this Java issue came about through the Windows update or the CW update. Anyway, here is the log:
eclipse.buildId=I20070613-1755
java.version=1.6.0_15
java.vendor=Sun Microsystems Inc.
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en
Command-line arguments: -os win32 -ws win32 -arch x86
!ENTRY org.eclipse.osgi 4 0 2014-01-09 16:04:25.978
!MESSAGE Application error
!STACK 1
java.lang.UnsatisfiedLinkError: Could not load SWT library. Reasons:
C:\Freescale\CW MCU v10.5\eclipse\configuration\org.eclipse.osgi\bundles\242\1\.cp\swt-win32-4236.dll: Invalid access to memory location
no swt-win32 in java.library.path
Can't load library: C:\Users\shaun\.swt\lib\win32\x86\swt-win32-4236.dll
Can't load library: C:\Users\shaun\.swt\lib\win32\x86\swt-win32.dll
C:\Users\shaun\.swt\lib\win32\x86\swt-win32-4236.dll: Invalid access to memory location
at org.eclipse.swt.internal.Library.loadLibrary(Library.java:331)
at org.eclipse.swt.internal.Library.loadLibrary(Library.java:240)
at org.eclipse.swt.internal.C.<clinit>(C.java:21)
at org.eclipse.swt.widgets.Display.<clinit>(Display.java:138)
at org.eclipse.ui.internal.Workbench.createDisplay(Workbench.java:653)
at org.eclipse.ui.PlatformUI.createDisplay(PlatformUI.java:161)
at org.eclipse.ui.internal.ide.application.IDEApplication.createDisplay(IDEApplication.java:154)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:96)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:110)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:79)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:353)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:180)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
at java.lang.reflect.Method.invoke(Unknown Source)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:630)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:585)
at org.eclipse.equinox.launcher.Main.run(Main.java:1439)
Hello James,
Under google I found some information regarding this error message.
Please have a look to:
Eclipse Community Forums: Newcomers » Hello World SWT - Could not load SWT library
I've MCU V10.5 and other version installed on Win 7 32 bit and Win 7 64 bit OS.
Both versions are running fine.
May be the problem occurs as the updates were done at same time.
Can you try to un-install windows updates ?
this could may be solved the problem.
Regards
Pascal
Hi Pascal,
It's fixed now. I was able to uninstall only 3 of the 5 updates, and had to reboot between each one, otherwise none of them would uninstall. CW10.5 started working again. I was then able to reapply the 3 updates and CW is still working.
Thanks for your help.
Regards,
Shaun