Am using an mc9s12xdt256, with CodeWarrior IDE 5.9.0
I have created 'bootstrap' code that resides in $E000 to $FFFF, and am placing application
code in $4004 to $D70F, and a secondary interrupt vector table in $D710 - $D7FF. The
bootstrap checks the CRC of the application area, and compares it with a PRM-calculated
checksum at $4000, and only jumps to the app if it is correct.
The PRM file segment definitions look like:
/* non-banked FLASH */
ROM_APP_CRC = READ_ONLY 0x4000 TO 0x4001;
ROM_APP_ENTRY = READ_ONLY 0x4002 TO 0x4003;
ROM_4000 = READ_ONLY 0x4004 TO 0xD70F FILL 0x3F;
ROM_VEC_TAB = READ_ONLY 0xD710 TO 0xD7FF FILL 0x3F;
a) If I use a single checksum entry calculation, from $4004 to $D70F, everything
works fine, and I jump to the app....
b) if I use a single checksum entry calculation anywhere beyond $D70F, it fails.
c) I tried using a two-entry checksum calculation in the PRM file, but - irrespective
of the endpoint of the 2nd stages calculation - it always fails.
Have attached a sample of one of my efforts.
CHECKSUM
CHECKSUM_ENTRY
METHOD_CRC16 INIT 0xFFFF POLY 0x1021
OF READ_ONLY 0x4004 TO 0xD70F
OF READ_ONLY 0xD710 TO 0xD7F9
INTO READ_ONLY 0x4000 SIZE 2
UNDEFINED 0x3F
END
END
It seems as if the automatically calculated checksum loses its
continuity at the segment change from ROM_4000 to ROM_VEC_TAB.
Is this an accurate asdsessment, and is there possible a workaround
for it?
I'd be very grateful for any assistance in this matter.
Seb
解決済! 解決策の投稿を見る。
- Did you verify that the flash content is correct other than looking at the checksum result? HIWAVE's load command can for example do a verify.
- The checksum fails as soon as it includes DF0A? What is at DF0A?
Does a 1 byte add checksum at DF0A fail?
- Which version of the tools are you using?
In the release notes of the linker 5.0.36 (in MCU10):
> - MTWX27784: Fix for an issue where linker calculates incorrect checksum with option -COCC
Daniel
Seb,
UNDEFINED 0x3F
When there's some gap between sections, some undefined addresses, CRC calculator uses UNDEFINED setttng to "fill" missing addresses. I wonder why did you change this to 0x3F? Erased flash state is all ones, or 0xFF for erased byte. Of course CRC should fail on unused locations, since they are 0xFF and CRC calculator assumed 9x3F. Change it back to 0xFF or remove optional UNDEFINED line.
Hi...
I use 0x3F for undefined areas as it is the opcode for a software interrupt
instruction, which I use to force a reset (processor has definitely gone astray
if it is trying to execute code in an undefined area). I also use it as the filler
byte for the segments.
It does work, in that the CRC is correct up to a point (up to $D709).
Ty for the suggestion, though... there's a couple of things that I can try out to
see what is actually happening, and shall post the results of my investigation.
Is going to be something very subtle, I think.. e.g. I found out that the PRM CRC
calculation does not work with an odd number of bytes (gives an error message!).
It's going to be something in the way that the calculation is performed.
Seb
Sorry for noise, I didn't notice FILL 0x3F.
First, the given version 5.9 is the version of the ide (the build system and editor). The most recent HC12 product version is 5.1 (I think). Are you using a recent version.
Then as the 2 segments are contiguous a single area should be fine. I never used the 2 areas syntax, I actually do not see the benefit of that compared with 2 separate checksums for distinct 2 areas. Either way, that's not your issue.
Did you verify that the content of the flash is indeed correct?
In order to narrow down the reason of the failure I would suggest to use a simpler checksum method (say add) and to narrow down the area which fails as much as possible, preferably to just a byte (or word for a 16 bit checksum). Then I would hope it gets obvious why it is failing...
Daniel
Hi...
I forgot to check the linker version, sorry...
I too prefer to use the single area syntax; I was thrashing around looking for a
solution.
Flash is correct, in that the CRC works well up to $D70F (DF09, actually).
I hadn't thought of using the 'add' method instead of 'crc-16' to narrow the list
of possibilities; I'll try that, and maybe 'xor-16' as well. That should provide some
clues.
Ty for the suggestion; shall update on my results.
Seb
- Did you verify that the flash content is correct other than looking at the checksum result? HIWAVE's load command can for example do a verify.
- The checksum fails as soon as it includes DF0A? What is at DF0A?
Does a 1 byte add checksum at DF0A fail?
- Which version of the tools are you using?
In the release notes of the linker 5.0.36 (in MCU10):
> - MTWX27784: Fix for an issue where linker calculates incorrect checksum with option -COCC
Daniel
Hi...
Sorry top be so late replying, but I felt the need to have a
break over Xmas.
I eventually settled on a single entry solution, and got the
thing going...
Your suggestion of using the command line option for the
fix seems to be exactly what I needed; I checked the release
notes, and it seems spot-on. Have put that on my to-do list
for tidying the software.
Thanks for your help, and hope that you (and the others) have
a happy new year,
Seb