Can't run hex file on FRDM-KE02Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't run hex file on FRDM-KE02Z

544件の閲覧回数
ngm
Contributor I

Hi,

I tried some demos from CW 10.6 and KDS 3.0 on the FRDM-KE02Z (Bootloader: V1.11 & App.Vers.: 1.14).

I used OpenSDA Embedded Debug-USB Port from CW 10.6 Trial.

I can flash and run the elf codes without problems.

The hex-codes, generated simultaneously with the elf-codes and flashed the same way, don't run.

I need some help

ラベル(1)
0 件の賞賛
返信
1 返信

419件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

how do you flash hex file to target? via simple flash tool "Flash to Target"?

please make sure you didn't use _host related library in your project:

pastedImage_0.png

if this can't help, please specify the steps to reproduce the problem step by step with your demo code.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信