Dear Sir,
I do configure CW for MC9S08AC60 controller but after saying FINISH it gives me following errors
Error occured while adding search path {Compiler}$$LIB_FOLDER$$\device\src
Make sure the path really exists!
Error occured while adding search path {Compiler}$$LIB_FOLDER$$\device\include
Make sure the path really exists!
Error occured while adding search path {Compiler}$$LIB_FOLDER$$\device\asm_include
Make sure the path really exists!
complete the last command: file 'main.c' cannot be added to target 'Standard'. You can look at the target's file mappings preference to see what file types it accepts
Error occured while adding file E:\rajan\projects\DemoProjects\Project_4\Sources\main.c to target.
complete the last command: file 'derivative.h' cannot be added to target 'Standard'. You can look at the target's file mappings preference to see what file types it accepts
Error occured while adding file E:\rajan\projects\DemoProjects\Project_4\Sources\derivative.h to target.
complete the last command: file 'MC9S08AC60.h' cannot be added to target 'Standard'. You can look at the target's file mappings preference to see what file types it accepts
Error occured while adding file D:\Program Files\bin\plugins\support\HC(S)08Wizard\Database\..\..\..\..\..\lib\hc08c\device\include\MC9S08AC60.h to target.
complete the last command: file 'ansiis.lib' cannot be added to target 'Standard'. You can look at the target's file mappings preference to see what file types it accepts
Error occured while adding file D:\Program Files\bin\plugins\support\HC(S)08Wizard\Database\..\..\..\..\..\lib\HC08c\lib\ansiis.lib to target.
complete the last command: file 'MC9S08AC60.C' cannot be added to target 'Standard'. You can look at the target's file mappings preference to see what file types it accepts
Error occured while adding file D:\Program Files\bin\plugins\support\HC(S)08Wizard\Database\..\..\..\..\..\lib\hc08c\device\src\MC9S08AC60.C to target.
I dont know what exactly problem is?
已解决! 转到解答。
Hello
You can find the latest release of CodeWarrior for HC08 from our Web page.
- Go to www.freescale.com/CodeWarrior
- Click on the link "RS08/HC(S)08 & ColdFire V1 Microcontrollers "
- Then click on the "Downloads" Tab
- Then click on the button "Download next to "Special Edition: CodeWarrior for Microcontrollers"
This release is automatically installed with a special edition license.
CrasyCat
Hello
Not sure which release of CodeWarrior you are using.
I checked my V6.2 installation and HCS08AC60 is fully supported in there.
So I would suggest you to upgrade to the latest release of CodeWarrior for MCU.
CrasyCat
Thank you!
I am using version v6.0 !And for controller AC16 it is showing option processor expert ! I have installed CW08_V5_1_HCS08_AC60_SP But i get only list of mmicrocontrollers !Would you give me link for proper service pack?Because AC32/AC48/AC60 these are the only three controller for which processor expert option is not been displayed in Wizard Map!
Hello
You can find the latest release of CodeWarrior for HC08 from our Web page.
- Go to www.freescale.com/CodeWarrior
- Click on the link "RS08/HC(S)08 & ColdFire V1 Microcontrollers "
- Then click on the "Downloads" Tab
- Then click on the button "Download next to "Special Edition: CodeWarrior for Microcontrollers"
This release is automatically installed with a special edition license.
CrasyCat