CW is giving me error for MC9S08AC60

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW is giving me error for MC9S08AC60

跳至解决方案
1,834 次查看
rajanjoshe
Contributor I

Dear Sir,

I do configure CW for MC9S08AC60 controller but after saying FINISH it gives me following errors

 

Error occured while adding search path {Compiler}$$LIB_FOLDER$$\device\src
Make sure the path really exists!


Error occured while adding search path {Compiler}$$LIB_FOLDER$$\device\include
Make sure the path really exists!


Error occured while adding search path {Compiler}$$LIB_FOLDER$$\device\asm_include
Make sure the path really exists!


complete the last command: file 'main.c' cannot be added to target 'Standard'.  You can look at the target's file mappings preference to see what file types it accepts
Error occured while adding file E:\rajan\projects\DemoProjects\Project_4\Sources\main.c to target.


complete the last command: file 'derivative.h' cannot be added to target 'Standard'.  You can look at the target's file mappings preference to see what file types it accepts
Error occured while adding file E:\rajan\projects\DemoProjects\Project_4\Sources\derivative.h to target.


complete the last command: file 'MC9S08AC60.h' cannot be added to target 'Standard'.  You can look at the target's file mappings preference to see what file types it accepts
Error occured while adding file D:\Program Files\bin\plugins\support\HC(S)08Wizard\Database\..\..\..\..\..\lib\hc08c\device\include\MC9S08AC60.h to target.


complete the last command: file 'ansiis.lib' cannot be added to target 'Standard'.  You can look at the target's file mappings preference to see what file types it accepts
Error occured while adding file D:\Program Files\bin\plugins\support\HC(S)08Wizard\Database\..\..\..\..\..\lib\HC08c\lib\ansiis.lib to target.


complete the last command: file 'MC9S08AC60.C' cannot be added to target 'Standard'.  You can look at the target's file mappings preference to see what file types it accepts
Error occured while adding file D:\Program Files\bin\plugins\support\HC(S)08Wizard\Database\..\..\..\..\..\lib\hc08c\device\src\MC9S08AC60.C to target.

 

I dont know what exactly problem is?

标签 (1)
标记 (1)
0 项奖励
1 解答
627 次查看
CrasyCat
Specialist III

Hello

 

You can find the latest release of CodeWarrior for HC08 from our Web page.

  - Go to www.freescale.com/CodeWarrior
  - Click on the link "RS08/HC(S)08 & ColdFire V1 Microcontrollers  "
  - Then click on the  "Downloads" Tab
  - Then click on the button "Download next to "Special Edition: CodeWarrior for Microcontrollers"

 

This release is automatically installed with a special edition license.

 

CrasyCat

在原帖中查看解决方案

0 项奖励
5 回复数
627 次查看
rajanjoshe
Contributor I
Also one more thing i noticed that for this microcontroller there is no processor expert option! Is it problem SP?
0 项奖励
627 次查看
CrasyCat
Specialist III

Hello

 

Not sure which release of CodeWarrior you are using.

 

I checked my V6.2 installation and HCS08AC60 is fully supported in there.

 

So I would suggest you to upgrade to the latest release of CodeWarrior for MCU.

 

CrasyCat

627 次查看
rajanjoshe
Contributor I

Thank you!

I am using version v6.0 !And for controller AC16 it is showing option processor expert ! I have installed  CW08_V5_1_HCS08_AC60_SP But i get only list of mmicrocontrollers !Would you give me link for proper service pack?Because AC32/AC48/AC60 these are the only three controller for which processor expert option is not been displayed in Wizard Map!

0 项奖励
628 次查看
CrasyCat
Specialist III

Hello

 

You can find the latest release of CodeWarrior for HC08 from our Web page.

  - Go to www.freescale.com/CodeWarrior
  - Click on the link "RS08/HC(S)08 & ColdFire V1 Microcontrollers  "
  - Then click on the  "Downloads" Tab
  - Then click on the button "Download next to "Special Edition: CodeWarrior for Microcontrollers"

 

This release is automatically installed with a special edition license.

 

CrasyCat

0 项奖励
627 次查看
rajanjoshe
Contributor I
thank you!
0 项奖励